Skip to main content

The Cab Command™ controller for Carrier Transicold’s Supra® truck refrigeration units has been redesigned for mounting in the dashboard, providing greater convenience and versatility for users. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

Offering the proven functionality of its predecessor, the new controller sports an attractive, intuitive interface in a refined compact design that conforms to the universal DIN specification, enabling simple and clean installation within a truck cab’s dash.

“Operators like the Cab Command controller because of its ease of use and functionality,” said Scott Parker, product manager, truck products, Carrier Transicold. “Our latest version offers the convenience of in-dash installation or, when used with an optional surface-mount bracket, it can be located on an overhead console, underneath or on top of the dash, giving users a wider range of placement options.”

The Cab Command controller features a bright, backlit LCD display that provides at-a-glance operating information, including setpoint, compartment temperature, operating mode and status. A smooth tactile keypad has logically arranged buttons for adjusting temperatures, changing operating modes and more.

The newly redesigned Cab Command controller is now standard for both single-temperature and multi-temperature Supra units. It is also backward compatible to earlier models. Plug-and-play operation makes installation easy for Supra unit owners who require a replacement controller or simply want to upgrade to the new version.

For more information about the Cab Command controller for Supra truck refrigeration units, turn to the experts within Carrier Transicold’s North America dealer network.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 45 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. For more information, visit www.transicold.carrier.com. Follow Carrier on Twitter: @SmartColdChain.

Carrier-Transicold-Truck-Trailer-New-Cab-Command-Controller-06282017-400x183
Carrier Transicold’s Cab Command™ controller for Supra® truck refrigeration units has been redesigned for convenient installation in a truck’s dashboard.