Skip to main content
Refrigeration
Carrier Transicold Launches [R]eCool: A 100% Electric Retrofit Solution Compatible with the Vector Range of Refrigeration Units for Trailers
Presented at Solutrans – Hall 4, Stand D065
Carrier-ReCool-CT
Carrier Transicold Launches [R]eCool: A 100% Electric Retrofit Solution Compatible with the Vector Range of Refrigeration Units for Trailers
Presented at Solutrans – Hall 4, Stand D065

At the Solutrans biennial trade show for road and urban transport professionals, Carrier Transicold unveils [R]eCool: a unique solution developed to convert existing Vector® diesel refrigeration units with E-Drive technology installed on semi-trailers into a 100% electric refrigeration solution powered by a high-capacity battery. Thanks to its exclusive E-Drive technology, the hybrid [R]eCool solution can also be recharged via the Vector's generator set. Carrier Transicold is part of Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions.

[R]eCool has been developed with the concept of reusing, reprocessing and recycling, offering substantial fuel savings and realistic, sustainable returns on investment. The retrofit solution is also available with the use of a secondhand battery, extending the life of the battery, supporting zero direct emissions and reducing waste.  

"Thanks to our 20+ years of experience of E-Drive electricity generation technology, Carrier Transicold is best positioned to offer this significant innovation,” said Victor Calvo, Vice President & General Manager, International Truck Trailer, Carrier Transicold. “[R]eCool enables our existing customers to convert their Vector diesel refrigeration units into a 100% electric, flexible and fully autonomous solution, perfectly suited to the constraints of urban traffic."

The objectives of the retrofit solution are to remove emissions directly linked to the use of diesel engines in refrigeration systems, including carbon dioxide, hydrocarbons, nitrogen oxides and particulate matter, and to considerably reduce noise emissions, allowing customers’ vehicles to enter low emission zones (LEZs). The solution also makes it possible to keep existing vehicles compatible with current and future climatic and regulatory guidelines.

[R]eCool is one of many solutions Carrier Transicold is displaying at the Solutrans tradeshow to further support its customers’ energy transition and decarbonization plans. Attendees can see Carrier Transicold’s latest innovations for trucks, trailers and light commercial vehicles at Hall 4, stand D065.

For more information about Carrier Transicold products and services, please visit www.carrier.com/truck-trailer/en/eu/.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled freight with a complete range of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing its customers around the world with environmentally friendly, efficient container refrigeration units and power generators, as well as light vehicle, straight truck and semi-trailer refrigeration units. Carrier Transicold is part of Carrier Global Corporation, global leader in intelligent climate and energy solutions that matter for people and our planet for generations to come. For further information, please visit https://www.carrier.com/truck-trailer/en/eu. Follow Carrier on X @SmartColdChain and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration