Carrier Transicold’s new, engineless 40XR and 50XR truck refrigeration units elevate the efficiency, reliability and sustainability of its direct-drive systems used for local and regional deliveries by grocery, food service, produce and pharmaceutical businesses. Carrier Transicold is a part of Carrier Global Corporation (NYSE: CARR), the leading global provider of healthy, safe, sustainable and intelligent building and cold chain solutions.
Along with contemporary aesthetics, the new XR series units provide improved air management and increased air flow resulting in faster pulldown and more uniform temperature control when compared to the X series models they succeed.
“The R in XR represents refinements we’ve made inside and outside to deliver greater performance and reliability,” said Scott Parker, Product Manager, Truck Products, Carrier Transicold. “For example, the unit condensers have been upgraded to our proven microchannel coil design for higher-efficiency heat transfer, as well as weight savings and added durability. Condenser fans have been enhanced with maintenance-free brushless motors for better reliability.”
“Sustainability is also improved when using the next-generation refrigerant R‑452A, which has about half the global warming potential of R-404A, the refrigerant used with the prior models,” Parker added. “Plus, due to efficiency gains, the required refrigerant is reduced by more than 20%.”
The XR series units are designed for mid-sized and large trucks. The 40XR, with an on-road capacity of 14,500 BTU/hour*, is designed for boxes 12 to 18 feet long. With a 17,000‑BTU/hour* on-road capacity, the model 50XR is well-suited to trucks with a cargo area up to 20 feet in length. Both models also have improved electric standby operation capacities compared to the models they succeed. As direct-drive units, their belt-driven refrigerant compressors are powered by the truck engine, eliminating the weight and costs associated with having a separate engine for the refrigeration unit.
Carrier Transicold direct-drive truck units are split systems, in which the condenser is nose-mounted to the truck box over the cab and the evaporator is attached to the ceiling of the cargo area. Carrier Transicold’s SlimLINE™ evaporator has an extra-flat, space-saving design that helps to maximize the cargo area. The refrigeration unit can be operated from within the driver cab via the easy-to-use Cab Command™ 2 digital control.
Carrier Transicold’s new XR series of engineless truck refrigeration units support Carrier’s aim to reduce its customers’ carbon footprint by more than one gigaton as part of its 2030 Environmental, Social and Governance goals. For more information about the 40XR and 50XR direct-drive truck refrigeration units, turn to the experts within Carrier Transicold’s North America dealer network.
About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, the leading global provider of healthy, safe, sustainable and intelligent building and cold chain solutions. For more information, visit Carrier Transicold. Follow Carrier on Twitter: @SmartColdChain, on Facebook at Carrier Transicold Truck/Trailer U.S. & Canada and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.