Skip to main content

For refrigerated haulers who require independent verification of temperatures inside trucks and trailers or immediate documentation for receivers, Carrier Transicold now offers the DataLink™ 2 recorder. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

For single-temperature or multi-temperature applications, the DataLink 2 system uses up to three independent temperature sensors, providing an added layer of verification beyond the refrigeration system’s built-in recording ability. An integral thermal printer lets drivers quickly and easily produce numerical and graphical trip reports for receivers. Additionally, data can be downloaded into a personal computer for electronic logging.

“Increasingly, haulers of pharmaceuticals, perishable and frozen foods, and other temperature-critical goods are using temperature monitoring and reporting capabilities, with temperature accountability a growing focus following the release of the transportation rules of the Food Safety Modernization Act,” said Mark Fragnito, product manager, controls, Carrier Transicold. “The DataLink 2 recorder may help food distribution operations easily track and manage this kind of information for compliance.”

Beyond its primary use as an independent temperature monitoring and reporting device, the DataLink 2 recorder provides additional advantages as a comprehensive analytical tool when connected to a Carrier Transicold refrigeration unit’s control system. Temperature data captured from its own sensors can be correlated against activities recorded by the control system, helping to identify potential sources of temperature excursions.

“Setpoint changes, defrost cycles, unit alarms, door openings and turning off the refrigeration unit can affect temperatures, and uniquely, the DataLink 2 recorder can capture and report these events alongside temperature data, providing helpful insight into temperature activity inside the truck or trailer,” Fragnito explained.

Designed for plug-and-play simplicity, the DataLink 2 recorder auto-detects which Carrier Transicold controller it is connected to, whether an APX™ or Advance® controller or the standard microprocessor. Setup is done through a “soft menu” system keyed to four buttons located just below the device’s backlit display screen. Two recorder styles are offered: body-mount models that attach to either a truck or trailer cargo area, and an in-dash DIN-mount version for more convenient driver access on straight truck applications.

For more information about the DataLink 2 recorder, turn to the experts within Carrier Transicold’s North America dealer network.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 45 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. For more information, visit www.transicold.carrier.com. Follow Carrier on Twitter: @SmartColdChain.