Carrier Launches Updated Line of Applied Rooftop Units
Now featuring lower-Global Warming Potential Puron Advance™ refrigerant
Charlotte, N.C. -
Carrier has launched a new line of K-Series WeatherMaker® Applied rooftop units available with more environmentally sustainable R-454B refrigerant, known commercially as Puron Advance. Carrier is a part of Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions.
The K-series is available in 20-to-60 ton nominal cooling capacities and features a robust indoor fan system and improved design for higher efficiency compared to legacy Carrier models.
The K-Series, which includes the 48K with gas heating and electric cooling and the 50K with electric cooling with optional electric or hydronic heat, has a commercial grade cabinet with fully hinged access panels, designed to fit most legacy Carrier curbs. The K-Series has a high-capacity forward curve indoor fan with variable frequency drive control and available Staged Air Volume or Variable Air Volume configurations to meet a wide range of application requirements.
Other features include Carrier SmartVu™ controls with a 7-inch touchscreen display, a refrigerant leak detection system with dissipation control, and a variety of factory installed options, including an ultra-low leak economizer, modulating gas or electric heat, Humidi-MiZer® dehumidification and double wall construction with available Agion® anti-microbial coating.
“Carrier’s K-Series rooftop units are the latest in a long line of flexible, efficient and reliable solutions for commercial air conditioning and indoor air quality needs,” said Michael Jones, Product Manager, Applied Packaged Systems, Carrier. “We’re helping our customers prepare to meet regulatory requirements while also designing our products to be efficient and innovative, all while offering easy installation and compatibility with existing curbs.”
The adoption of Puron Advance surpasses the EPA’s lower GWP requirements for 2025. R-454B has a GWP100 of 466 according to the Intergovernmental Panel on Climate Change Fourth Assessment Report — a 75% reduction from R-410A — and non-ozone depleting potential, the refrigerant was selected as one of the best solutions to minimize environmental impact and provide longevity based on the United Nations Montreal Protocol Kigali Agreement phasedown plan. GWP is a measure of a substance’s climate warming impact compared to CO2.
For more information on Carrier and the WeatherMaker line of Applied rooftop units, visit https://www.carrier.com/commercial/en/us/.
About Carrier
Founded by the inventor of modern air conditioning, Carrier is a world leader in high-technology heating, air-conditioning, digital platforms and building automation systems. Carrier experts provide sustainable solutions, integrating energy-efficient products, controls and service for commercial applications, including data centers, healthcare facilities, schools, retail centers, office spaces and more. Carrier is a part of Carrier Global Corporation, global leader in intelligent climate and energy solutions that matter for people and our planet for generations to come. For more information, visit https://www.carrier.com/commercial/en/us/ or follow us on LinkedIn and @Carrier on X.