Skip to main content

Carrier Energy Demand System Provides Automated Energy Management

SYRACUSE, N.Y. -

Carrier has released its Energy Demand System, which creates a wireless network of automated demand-management and demand-response controllers that can be installed onto any packaged rooftop unit. Utilizing patented intelligence, the system can dramatically reduce peak electrical demand by up to 30 percent in commercial and light commercial properties and allow for effective scheduling of overnight and weekend loads. Carrier, the world’s leader in high-technology heating, air-conditioning and refrigeration solutions, is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp. (NYSE: UTX).

Controllers within the wireless network broadcast unit power readings to each other every 30 seconds, and each controller is capable of making the decision to run or delay unit operation every few minutes to ensure the most effective use of energy. Plus, a gateway provides two-way Internet communication without the need to access the site’s Internet connection. Power readings and controller decisions are uploaded to the server every five minutes for data logging and analysis.

The Carrier Energy Demand System is as easy to install as a thermostat and requires no special training. Once installed, the controllers work together to intelligently communicate and manage the duty cycle of the units being controlled, which makes this an ideal solution when a full-building automation system is not required.

In addition, the Energy Demand System is demand-response-capable and OpenADR compliant, which allows for systematic load shedding when requested by utilities or energy aggregators.

“The Carrier Energy Demand System is an ideal solution when a building does not require full automation, but there is a need to control electrical demand across several rooftop units,” said Greg Alcorn, vice president, commercial sales and marketing, Carrier. “The controllers are easy to install and seamlessly connect with one another to provide the building owner with a reliable and effective energy management system.”

To learn more about Carrier’s Energy Demand System, visit www.commercial.carrier.com. Follow the company on Twitter: @CarrierGreen.

ABOUT CARRIER

Founded by the inventor of modern air conditioning, Carrier is the world’s leader in high-technology heating, air-conditioning and refrigeration solutions. Carrier experts provide sustainable solutions, integrating energy-efficient products, building controls and energy services for residential, commercial, retail, transport and food service customers. Carrier is a part of UTC Building & Industrial Systems, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. For more information, visit www.carrier.com or follow @CarrierGreen on Twitter.