Get Ready for EcoDesign with Carrier!
On the cabinets:
Each new refrigerating appliance will be supplied with a printed label gathering energy related information. It is then up to the retailer to display the label in the store or not.
Centralized for all suppliers:
All suppliers are requested to enter their product labels into a European product database called EPREL.
On promotion material:
Any visual advertisement for a specific model must contain the energy efficiency class and the range of energy efficiency classes available on the label.
The following information shall be included in the label:
I. QR code;
II. Supplier's name or trademark;
III. Supplier's model identifier;
IV. Scale of energy efficiency classes from A to G;
V. The energy efficiency class determined;
VI. Annual energy consumption AE in kWh per year;
VII. The sum of the display areas with chilled operating temperatures, expressed in square meters (m²);
VIII. The temperature at the top: the highest temperature of the warmest M-package of the compartment(s) with chilled operating temperatures, in degrees Celsius (°C) or the temperature at the bottom: the lowest temperature of the coldest M-package of the compartment(s) with chilled operating temperatures, in degrees Celsius (°C) or the highest minimum temperature of all M-packages of the compartment(s) with chilled operating temperatures, in degrees Celsius (°C)
IX. The sum of the display areas with frozen operating temperatures, expressed in square meter (m²) and rounded to two decimal places;
X. The highest temperature of the warmest M-package of the compartment(s) with frozen operating temperatures, in degrees Celsius (°C)
The lowest temperature of the coldest M-package of the compartment(s) with frozen operating temperatures, in degrees Celsius (°C) or the highest minimum temperature of all M-packages of the compartment(s) with frozen operating temperatures, in degrees Celsius (°C)
XI. The number of this Regulation, that is ‘2019/2018’
![question-mark-graphic question-mark-graphic](https://images.carriercms.com/image/upload/w_180,c_lfill,f_auto/v1605691690/carrier/commercial-refrigeration/miscellaneous/question-mark-graphic.png)
I have a question!
Does the energy label need to be visible for the consumers in the shops?
Refrigerated cabinets need to be delivered with the energy label by the supplier. The Regulation directive doesn’t mention the need for shops to have it visible or sticked on the product.
#GetReadyForEcoDesign #CarrierAtYourSide #EcoDesign #EnergyEfficient