*Depending on the cabinet model and/or mechanical system, as well as optional equipment selected during configuration and different environmental conditions, the energy saving potential for the cabinet and/or mechanical system you are using may deviate. The values given are comparisons between the operation of the cabinets and/or mechanical systems without and with the additional services offered through the Carrier Energy Optimization Program (referred to as "Energy Savings Solutions").
Carrier Commercial Refrigeration Energy Optimization Program
Delivering Energy Efficiency and Sustainable Savings
With sharp increases in energy costs globally, Carrier has launched its Energy Optimization Program aiming to deliver sustainable savings. Carrier is committed to providing customers with energy efficient solutions that maximize merchandising opportunities and reduce their carbon footprint. When partnering with Carrier, you can be sure that energy efficiency and sustainability are at the heart of our products and solutions.
Carrier has proven, ready-to-install products to help customers reduce their energy usage by as much as 40%*, while also reducing their carbon footprint.
Carrier has a broad portfolio of EcoDesign-compliant products and solutions to provide businesses – from small commercial applications to large industrial installations – access to an array of modern energy and cost-efficient technology.
On-site Energy Evaluations
As part of this program, Carrier will offer on-site energy evaluations during which our team will provide custom recommendations on how to reduce energy consumption at the customer site.
Please contact our sales team at [email protected] to learn more about the Carrier Energy Optimization Program and how we can help reduce your energy costs today.
We understand the uncertainty our customers are experiencing with the recent spike in energy prices and that they’re looking for ways to control costs.
An easy way to reduce energy consumption is to upgrade existing equipment. Carrier´s modernization solutions offer the latest in energy-saving products. Energy-saving upgrades can be easily installed on the existing refrigeration equipment and can achieve up to 35%* of energy savings.
Carrier offers energy-saving upgrades for a wide range of installed equipment at both store and system levels. As part of the Energy Optimization Program: Delivering Sustainable Solutions, Carrier will offer on-site energy evaluations during which highly trained Carrier teams will provide recommendations on how to reduce energy consumption at the customer site.
In store retrofit
Glass doors |
Glass lids |
Shelf edge technology |
LEDs |
Open cabinets consume more energy than closed cabinets. Installing glass doors, followed by a quick post-installation fine tuning can save up to 30%* energy consumption. | Glass lids are available for open island chillers and can offer energy savings up to 20%*. | The shelf edge is an innovative technology developed through the detailed airflow analysis in the cabinet. Double blades in the shape of a venturi regulate the airflow, minimize the cold air spillage and save up to 20%* energy per cabinet. Shelf edge blades are an alternative option to the glass doors and can be installed easily on the shelves. | Replacing older-generation LEDs with new LED technology offers considerable energy savings. |
Systems
Subcooler/desuperheater |
Air curtains |
Spray systems |
Carrier offers a wide range of standard and configurable subcoolers and desuperheaters to support customers' installed equipment. | A high amount of energy is lost during frequent opening and closing of cold storage doors. Most of the cold storage in retail markets operate in hot and humid zones. Hot ingress into cold storage brings a lot of moisture, which builds ice in the evaporator, door hinges, roof and flooring. Using air curtains can reduce moisture ingress and energy losses. | With time, condensers and gas coolers lose their capacity over time resulting in high energy consumption. The spray and mesh system cools the incoming air, increases condensing capacity and saves energy. |
For even more modernizations for your refrigeration needs, see our full range of offerings HERE.
At Carrier, we incorporate sustainability into all we do, and we strive for energy efficiency in our refrigeration cabinets.
Our perfectly fit glass door design can make a significant reduction in the overall cabinet energy consumption in a supermarket. If customers prefer open cabinets, we can optimize energy efficiency with motorized, highly efficient night blinds and other features.
BREEZtec is our new standard when it comes to air circulation und fan efficiency. With state-of-the-art LEDs we can optimize energy consumption for cabinet lighting.
Cabinets
High-efficiency glass doors |
BREEZtec air circulation technology |
Night curtains |
High-efficiency LEDs |
Energy efficient refrigeration systems:
- Reduced compressor electrical consumption leading up to 30% energy saving compared to traditional CO2 systems: Patented modulating vapor ejector combined with flooded mode
- Valorization of heat rejected by the refrigeration process: Heat reclaim for tap water / floor heating
Energy efficient heating systems:
- Our technology and experience of refrigeration at the service of heating. We offer high-temperature heat pumps, providing hot water up to 90°C with CO2 natural refrigerant
- Heat pumps have a better efficiency performance than gas boiler or electrical heaters (from 1.5 to 5 times better)
- The best route to reduce the heating energy bill and hit your decarbonation road map target
- Heating capacities from 50kW to 2.2MW
Combination of both heating and cooling at the same time:
- Our water-cooled chiller and water source heat pumps functions can be combined on the same unit, embedding smart control to manage cooling and heating demand
High-efficiency systems
Ejector combined with flooded system and heat recovery
Heat pumps to supplement or replace gas boilers
Click here to learn more
Carrier is expanding digital services with a specific energy management offering based on three pillars.
Digital energy management elevates the offering to a new level by offering constant optimization always based on current conditions. Typically, digital offerings come with a limited investment needed in hardware.
Carrier expanded digital services:
- Demand and supply side energy management
- Refrigeration system efficiency
- Store system efficiency