![carrier-case-study-citi-group-tower-london_h](https://images.carriercms.com/image/upload/w_auto,h_400,c_fill,g_center,q_auto,f_auto/v1606827844/carrier/commercial-hvac-europe/case-studies/uk/carrier-case-study-citi-group-tower-london_h.jpg)
CITIBANK - Banking
![carrier-map-case-study-uk](https://images.carriercms.com/image/upload/w_auto,dpr_auto,c_limit,q_auto,f_auto/v1571219275/carrier/commercial-hvac-europe/graphics/carrier-map-case-study-uk.png)
![carrier-case-study-citibank-centrifugal-chiller-in-plant-room-1](https://images.carriercms.com/image/upload/w_auto,dpr_auto,c_limit,q_auto,f_auto/v1606827844/carrier/commercial-hvac-europe/case-studies/uk/carrier-case-study-citibank-centrifugal-chiller-in-plant-room-1.jpg)
Project description
In their efforts to help customers manage energy consumption and operational costs, Carrier engineers added Greenspeed® intelligence for Variable Speed Drive (VSD) functionality to two Carrier AquaEdge,sup>™ 19XR5 centrifugal chillers serving Citi’s UK headquarters at Canary Wharf, London. Power use was monitored before and after deployment of Greenspeed® intelligence, demonstrating substantial reductions in energy consumption, and proving the case for such VSD retrofits.
Background
The Citi retrofit project was carried out in two stages. Stage one involved installing Greenspeed® intelligence on the first centrifugal chiller. To help the customer quantify the benefit in terms of lower energy consumption and reduced running costs, Carrier monitored energy use before and after installation using Carrier’s IVU system. The tracking showed substantial energy savings as a result of the use of variable speed drives, encouraging Citi to request the installation of a second centrifugal chiller with Greenspeed® intelligence.
Following completion of stage two, Carrier monitored actual performance data for the two chillers with Greenspeed® intelligence, and compared the data with previous energy consumption figures prior to retrofitting. The results enabled savings of £33,966 for the first three months of 2013, in line with projections and proving the case for the retrofit of variable speed drives.
![carrier-case-study-citibank-centrifugal-chiller-in-plant- room-2 carrier-case-study-citibank-centrifugal-chiller-in-plant- room-2](https://images.carriercms.com/image/upload/w_300,c_lfill,f_auto,q_auto/v1606827856/carrier/commercial-hvac-europe/case-studies/uk/carrier-case-study-citibank-centrifugal-chiller-in-plant-room-2.jpg)
- Operational savings through reduced energy consumption
- Optimized environmental impact with lowered carbon emissions
- Reduced service maintenance requirements: less wear and tear due to “soft start” and “soft stop” functions
- Creation of productive building environment for occupants: chiller delivering very stable comfort conditions
- Reduction noise emission: ability to adapt the speed of compressor motors to the current cooling demand thus avoiding constant full speed operating
- 2 X AquaEdge™ 19XR5 centrifugal chiller
- Carrier custom designed and built Greenspeed® intelligence variable speed drives
- Updated version of Carrier’s Interface Chiller Visual Control (ICVC) and software package, with Integrated Starter Module
The solution addressed a number of specific challenges:
- A custom-made variable speed drive: An off-the-shelf, ready-made variable speed drive solution was not available for the chillers. Therefore, Carrier designed and built a custom solution, matched to the exact requirements of the project. Greenspeed® intelligence reduces chiller energy consumption by adjusting cooling capacity to match the current load. At the outset, Carrier calculated that the energy savings for both chillers retrofitted with Greenspeed® intelligence would be in the region of £126,000 a year.
- A re-assembly on-site: Carrier responded to the installation site ceiling height limitations by delivering the system in several modules which were assembled once in position.