Skip to main content

Carrier AquaEdge 19DV Chiller Line Expands to 3850kW

MONTLUEL, France -


Carrier today announced that it has expanded its award-winning AquaEdge® 19DV water-cooled centrifugal chiller capacity range in Europe. With capacity now up to 3850 kW, the AquaEdge 19DV can accommodate customer requirements of higher capacity applications such as commercial high-rise and mixed-use buildings, large manufacturing factories and healthcare facilities. The AquaEdge 19DV is the ultimate innovation in chiller technology and utilizes a refrigerant with an ultra-low global warming potential of ~1. Carrier is a part of Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions.

"The AquaEdge 19DV is built on the legacy of Willis Carrier’s breakthrough invention of the centrifugal chiller, which recently celebrated its 100th anniversary," said Tom Franaszek, Director, Global Product Management, Water-cooled Chillers, Carrier Commercial HVAC. "The 19DV’s unique EquiDrive two-stage back-to-back compressor design improves efficiency and operating range, continuing Carrier’s technological leadership in centrifugal chiller design."

The AquaEdge 19DV was designed to minimize environmental impact while also providing industry leading efficiency. It also provides free cooling, a strategy for leveraging natural air temperatures, which can result in meaningful energy costs savings per year while reducing maintenance costs and mechanical room space. The efficient design supports Carrier’s 2030 ESG goal to reduce its customers’ carbon footprint by more than 1 gigaton.

Additional features include a variable frequency drive (VFD) that protects the chiller against abnormalities in the power quality being delivered to a system. In addition, every 19DV is supported by Carrier’s BluEdge™ service platform, providing actionable analytics and real-time dashboards. Carrier Service automatically trends, predicts and analyzes performance, allowing for a strategic approach to preventive maintenance and providing an intuitive way to monitor plant energy consumption.

The innovative AquaEdge 19DV launched in Asia in 2016 before introduction to other regions, earning a reputation for reliability and efficiency. The chiller has amassed more than five international accolades, including earning gold in the U.S.-based Consulting-Specifying Engineer Product of the Year Awards, Boilers & Chillers category and the RAC Cooling Industry Award for Air Conditioning Product of the Year in the System/Standalone category in London.

To learn more about the Carrier AquaEdge 19DV water-cooled centrifugal chiller, visit 19DV.


carrier-aquaedge-19dv

With capacity now up to 3850 kW, the AquaEdge 19DV can accommodate commercial high rise and mixed use buildings, large manufacturing factories and healthcare facilities. The AquaEdge 19DV is the ultimate innovation in chiller technology and utilizes a refrigerant with an ultra-low global warming potential of ~1.