ICC Wales - Convention Centre


Project description
Carrier’s award-winning high efficiency AquaForce® Vision 30KAV chiller has been chosen to provide high quality air conditioning for the new International Convention Centre Wales (ICC Wales).
Two Carrier 30KAV chillers equipped with Greenspeed® Intelligence inverter-driven screw compressors have been selected to air condition the new facility, each delivering 791kW of cooling. The innovative technology recently won the Air Conditioning Product of the Year 2018 in the UK’s Cooling Industry Awards, due to its energy efficiency and excellent environmental credentials. The chillers are being deployed in a duty share configuration, with each chiller sized for 58% of the diversified load to provide outstanding resilience and continuity of cooling at all times.
Background
Located at the prestigious Celtic Manor Resort, host of the Ryder Cup and recent NATO Summit, the ICC Wales project is an £83.7m joint venture between the resort’s owners and the Welsh Government. The new venue, which opens in 2019, will accommodate 5,000 delegates and includes a 4,000sqm pillar-free main hall, a 1,500 seated auditorium, 12 flexible meeting rooms, a double-height glass atrium and a 2,500sqm plaza for outdoor events.
Peter Davies, director of contractor and installer CMB Engineering, said:
“Carrier has a reputation for reliable, well-engineered systems, and the company’s senior sales engineer Russ Tyrell provided helpful support throughout the project. The efficiency performance of the new 30KAV chiller range is excellent due to the use of inverters that precisely match cooling output to current load. This is highly attractive for end users, as it delivers high quality comfort conditions for occupants, while minimizing running costs and enhancing environmental credentials, all important considerations in the ICC Wales project.”

- High energy efficiency
- Excellent environmental credentials
- Outstanding resilience and continuity of cooling at all times
- 2 X Carrier 30KAV chillers, equipped with Greenspeed® Intelligence inverter-driven screw compressors