i-Vu® BACnet® Scheduling Interface Add-On
ADD-SCH-BACNET
Carrier® i-Vu® add-ons extend the capability of the i-Vu building automation system.
The BACnet Scheduling Interface add-on allows third-party event management software to write BACnet schedules to the i-Vu building automation system. These schedules can then be used to tell mechanical equipment when to run in the building.
Often times building operators may use operations management software to maintain a single calendar of events for a facility. This add-on provides them with a seamless integration to the building automation system so that they can manage comfort conditions and/or lighting systems in the building during scheduled events. When BACnet schedules are written through this add-on, building operators are also able to manage the schedules using the i-Vu user interface.
Allows the i-Vu building automation system to be scheduled via third-party BACnet software such as:
- SchoolDude® - Operations Management Software
- Events2HVAC™ - Event Automation Software
- Hospitality Scheduling Software
- i-Vu Pro 6.5 or later user interface with latest cumulative update (CIV-OPNPR or CIV-OPNPRUL)
- Software is configured with at least one active BACnetIP connection
- Licensed BACnet Scheduling Interface Add-on
- Third-party BACnet software must meet BACnet protocol revision v4 or later, including clients that support the K.3 BIBBs: SCHED-A, SCHED-AVM-A, SCHED-VM-A.
Allows the i-Vu building automation system to be scheduled via third-party BACnet software such as:
- SchoolDude® - Operations Management Software
- Events2HVAC™ - Event Automation Software
- Hospitality Scheduling Software
- i-Vu Pro 6.5 or later user interface with latest cumulative update (CIV-OPNPR or CIV-OPNPRUL)
- Software is configured with at least one active BACnetIP connection
- Licensed BACnet Scheduling Interface Add-on
- Third-party BACnet software must meet BACnet protocol revision v4 or later, including clients that support the K.3 BIBBs: SCHED-A, SCHED-AVM-A, SCHED-VM-A.