To find your Carrier Authorised Service Provider, download the ContainerLink™ app.

Carrier Transicold Adds High-Performance PowerLINE Generator Sets Compliant with EU Emission Standards for Enhanced Sustainability

Singapore -

Carrier Transicold has expanded its portfolio of PowerLINE® generator sets for refrigerated containers with new Series 55 models designed for compliance with European Union Stage V standards for diesel engines, offering greater sustainability. Carrier Transicold is a part of Carrier Global Corporation (NYSE: CARR), the leading global provider of healthy, safe and sustainable building and cold chain solutions.

“In addition to providing efficient performance that our customers in Europe have come to expect, our new PowerLINE Series 55 models use a familiar engine style and a new permanent-magnet generator to deliver reliability and simplicity of operation,” said Charu Mahajan, Associate Director for Generator Sets, Global Container Products, Carrier Transicold. “Recommended for European applications, the Series 55 bears the CE mark, and its 18.5 kW engine complies with Europe’s Stage V nonroad mobile machinery emissions standard, which includes low thresholds for carbon monoxide, hydrocarbons, particulate matter and nitrogen oxides.”

The combination of a fuel-efficient diesel engine, built-in FuelWise™ two-speed functionality and the new ultra-high-efficiency generator results in a reliable, uninterrupted electrical source for refrigerated containers when transported over land via truck or rail. The generator features a single-winding, contactless architecture for reduced complexity and enhanced reliability.

Key differentiators of the new PowerLINE Series 55 model:

  • Compliant with European Union Stage V standards for diesel engines
  • Full operating power to start and run ISO reefers across operating envelope
  • Simple, reliable design featuring familiar engine style and ultra-high efficiency generator, making it easy to use and operate
  • 2-speed controller automatically switches based on conditions corresponding to refrigeration system load and requires no user interaction
  • Carrier-exclusive FuelWise feature delivers fuel savings of up to 34% when hauling perishable and frozen commodities at typical refrigerated setpoints, which is 6% better than legacy PowerLINE generator sets with FuelWise

 “By reducing fuel consumption, distances traveled on the same tank of fuel are extended,” said Mahajan. “Likewise, carbon footprint per trip is reduced through fuel conservation and a commensurate reduction in emissions.”

PowerLINE Series 55 generator sets are part of Carrier’s Healthy, Safe, Sustainable Cold Chain program, which provides fresh foods and medications to people around the world and ensures the safe storage and transport of critical vaccines through advanced connectivity and visibility. Learn more at corporate.carrier.com/healthycoldchain or visit transicold.carrier.com.

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, the leading global provider of healthy, safe and sustainable building and cold chain solutions. For more information, visit transicold.carrier.com. Follow Carrier on Twitter: @SmartColdChain or on LinkedIn at Carrier Transicold Container Refrigeration.

Carrier Transicold’s latest PowerLINE generator sets for refrigerated containersCarrier Transicold’s latest PowerLINE generator sets for refrigerated containers, such as this undermount version, are designed specifically for use in Europe and are compliant with the strict Stage V emissions standards.