Skip to main content

Carrier Transicold Iceland and Supra Units Help BAKO Cut Fleet Emissions

WARRINGTON, England -

Bakery wholesaler BAKO has taken delivery of 24 new rigid trucks, mounted with a combination of Carrier Transicold Supra 1150 MT (multi-temperature) systems and engineless Iceland 11 MT units. The trucks will deliver powerful and efficient cooling capability, with the ability to power the refrigeration units via the truck’s engine and help reduce fuel usage and deliver potential emissions savings. Carrier Transicold is a part of Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions.

BAKO’s new Carrier Transicold Iceland MT units are each fitted to 18-tonne and 26-tonne Scania L-320 rigid trucks, supplied by Preston Scania. In addition, the new Supra 1150 MT units, mounted to 26-tonne Volvo FM rigids, feature insulated box bodies built by Gray & Adams. They replace older vehicles in the company’s temperature-controlled fleet, while the move represents the first time BAKO has selected Carrier Transicold’s engineless technology.

“No matter the type of unit, we have always found that Carrier Transicold offers one of the most complete packages in relation to innovation, performance, price and product availability,” said Tony Cookson, Transport Manager at BAKO. “We’re excited to see how Carrier’s engineless technology will help the business through reducing fuel costs, as well as delivering excellent sustainability benefits through reduced emissions and significantly quieter operation.”

Carrier Transicold’s Iceland units run on power derived directly from the truck’s own engine through the company’s innovative Eco-Drive system. Eco-Drive incorporates a hydraulic pump connected to the vehicle’s engine power take-off, which is capable of generating the electrical input required to provide 100% refrigeration capacity, even at standard idle speed. The Iceland unit also boasts rapid temperature pull-down capability and operates at a PIEK-compliant level below 60 dB(A).

Removing the need for a separate diesel engine to function, the new Iceland units also contribute to Carrier’s Environmental, Social & Governance (ESG) goal of helping its customers avoid more than one gigaton of greenhouse gas emissions by 2030.

BAKO’s new Supra 1150 MT units mounted on rigid trucks have also been fitted with Eco-Drive systems, creating a hybrid set-up that allows the company to switch back to the Supra unit’s standalone diesel power if the vehicle stops for any period of time, without the need to keep the truck engine running.

“It’s been a delight to work with the BAKO team on the supply of its new rigids and to introduce them to the power of the Eco-Drive, Iceland and Supra systems,” said Geoff Fearnley-Hill, National Key Account Manager, Carrier Transicold UK. “We’re proud that our technology will allow the business to combine outstanding performance with superb sustainability benefits moving into the future.”

BAKO’s new products are also all backed by Carrier Transicold’s comprehensive BluEdge fixed cost full-service maintenance package. This includes annual temperature control testing and certification, full regulatory checks and access to the company’s oneCALL 24/7 incident management service.

For more information on Carrier Transicold products and services in the UK, visit www.carriertransicold.co.uk. Follow Carrier Transicold on X: @SmartColdChain or on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.

 

About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, global leader in intelligent climate and energy solutions that matter for people and our planet for generations to come. For more information, visit www.carriertransicold.co.uk. Follow Carrier on X: @SmartColdChain and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.