Your Guide To Gas Furnace Replacement
In the United States, natural gas furnaces are the heating systems of choice for many families. It’s easy to see why. They are efficient, effective, and there’s nothing like the warm, cozy feeling of heated air coming from the registers on a cold, winter day.
But what happens when your furnace’s performance doesn’t leave you so warm and fuzzy? Before your mind goes right to gas furnace replacement and its annoying sibling, gas furnace replacement cost, there’s a lot to consider. Sometimes, your system just needs a tune-up or a minor repair. Other times, especially if it’s older, a major expense might be looming.
If “furnace replacement” does find its way to the top of your to-do list, this article is for you. We'll cover the basics, like when to replace gas furnaces, what is the average cost to replace gas furnaces, what additional expenses might be associated with replacing furnaces, and other details to consider.
While it might be sad saying goodbye to your trusty old heater, saying hello to one of the many Carrier gas furnaces available can warm your heart and open the door to improved comfort and energy efficiency.
When to Get A Furnace Replacement
You can expect a gas furnace to provide 15-20 years or more of reliable operation. But what happens if you start noticing increased energy costs, strange sounds coming from your system, or your home just isn’t staying very comfortable? Even the most dependable heating system will eventually need to be replaced. And all too often, it happens in the middle of winter, when it’s an emergency, when HVAC technicians are busy, or when your choices are limited to available stock. So, when are the best times to replace gas furnaces?
Ideally, try to have your new furnace installed in the spring or summer – when you don’t need the furnace immediately for heating. This will give you a little more time to weigh your options, and maybe even save a little money too. Here are some signs that a new furnace might be a good idea:
- Repairs are becoming more frequent and more expensive
- Your furnace is showing signs of malfunction, such as:
- making weird noises
- showing signs of rusting or cracking
- emitting dust or soot
- smells funny when running
- running constantly
- turning on an off more frequently
- Heating energy bills are getting higher for no apparent reason
- Heating in the home is worse than before or uneven
These issues may just mean that your furnace needs some basic maintenance or a minor gas furnace repair. They could also mean your furnace is getting to the end of its lifespan and needs to be replaced, especially if the repairs are getting expensive compared to the cost of a new one. If you are concerned, now would be a great time to contact your local Carrier expert to assess the situation.
How Much Does A Furnace Replacement Cost?
Gas Furnace Replacement Cost
The cost to replace gas furnaces can vary quite a bit. A new gas furnace can have average costs ranging from $3,800 to $12,000. These price ranges depend upon the types of furnaces and whether installation costs are included. For example, a basic, single stage unit without installation will cost quite a bit less than a highly efficient furnace with materials and labor charges included. Other factors that can impact the gas furnace cost include the size (heating capacity), comfort-enhancing features like variable-speed fans or multi-stage heating, and efficiency-enhancing features like a secondary heat exchanger.
Electric Furnace Replacement Cost
Fuel source can affect pricing as well. The initial cost for an electric furnace, including installation, is typically less than the cost for a similarly sized gas furnace with installation but the ongoing heating costs for an electric furnace could cost significantly more money, especially in colder climates.
Additional Gas Furnace Replacement Costs
As you narrow down the choices for your new heating system, it’ll be important to budget for all of the associated gas furnace replacement costs. Labor, materials, permits, inspections and any additional equipment like indoor air quality accessories can really add up.
- Labor costs for the installation are a given, unless you are a trained HVAC professional and can do it yourself. For a licensed HVAC technician, expect to pay around $50 - $100 per hour1 , and you will likely have more than one person on the crew which will incur additional fees. Of course, a bigger crew can get the job done faster.
- If the current setup doesn’t work for your new furnace, expect to add new ductwork and/or ventilation to your installation cost. Charges could be minimal if only simple modifications are needed. For a more extensive job, or installing new ductwork for the entire home, you can expect to pay quite a bit more.
- Some states or municipalities may require special permits, inspections or both. If required, you might expect to pay anywhere from $400 - $1,500.2
- Increasing the size (heating capacity) of your furnace can increase the cost of your furnace as well. This might be the case if your old one is undersized, or if a larger unit is needed to accommodate additional heating for a room addition.
- Indoor air quality accessories such as a whole-home humidifier, air purifier and UV lamps are often installed with a new furnace. These types of accessories can be added later, but it is usually more cost-effective to include them during the furnace installation.
What to Consider for a Furnace Replacement
While price is important, there are other factors to consider when shopping for a gas furnace replacement. You’ll get your best value when you choose a model that provides benefits beyond basic heating. Here are some factors to think about as you balance initial budgeting concerns with long-term value and satisfaction:
Correct furnace size
Your HVAC technician should be able to assess your home and calculate the heating capacity you’ll need to keep comfortable. This determines the correct furnace size. Don’t just assume your old system was sized correctly – that might be why you are shopping for a new one! Learn more about calculating furnace size.
Newer furnace technology
Today's furnaces can include a number of features that make heating more consistent and energy efficient. Variable-speed models can smooth out airflow to more evenly distribute heat. They can also help dehumidify during the summer months as part of your cooling system. Multi-stage models can adjust heating capacity as needed to improve both comfort and fuel economy.
Furnace efficiency
A high efficiency furnace might cost more up front but can save money on heating bills for the life of the unit. How do you determine a furnace's efficiency? Annual Fuel Utilization Efficiency, or AFUE. The higher the AFUE, the more efficient the furnace is. Consider a high AFUE furnace or ENERGY STAR® certified model. High efficiency furnaces might qualify for local utility company rebates or federal tax credits.
Furnace modulation

Connect With A Carrier Professional For Furnace Replacement Near Me

Explore Carrier Furnaces
ENERGY STAR® certified. Up to 97.0% AFUE for premium energy savings with enhanced comfort features.
ENERGY STAR® certified. Up to 97.0% AFUE for premium energy savings with enhanced comfort features.
All sizes ENERGY STAR® certified. Up to 97% AFUE for premium energy savings with standard comfort features.
Frequently Asked Questions About Gas Furnace Replacement
Replacing a gas furnace is a bit more complicated than getting a new refrigerator or washing machine. It’s a topic that generates a little more anxiety and a few more questions than other appliances. Here are a few frequently asked questions we hear on a consistent basis:
Replacing a furnace isn’t a recommended DIY type of project. HVAC contractors receive special training on the many aspects of installation, including how to properly and safely connect natural gas lines, electrical wiring and venting. All must be done correctly and according to local building codes to ensure safe operation.
A typical, standard installation with minimal modifications to ductwork should take around a day. A more complex installation with new ductworkand other components like an air conditioner or air purifier can take longer.
Try to clear a path through your home to make bringing in your new furnace and removing the old one easier. Secure pets so they don’t get out or get in the way. Put down a drop cloth or tarp over carpeting/flooring near the installation area.
Yes, you might want to consider replacing a 20-year-old furnace, as the average life expectancy of most furnaces today is between 15 and 20 years. If your furnace is nearing or surpassing this age, it’s likely less efficient than newer models and more prone to breakdowns, so it's wise to start shopping for a new, energy-efficient model before it fails completely.
A furnace typically needs to be replaced every 15 to 30 years, depending on its maintenance and usage. Most furnaces begin to lose efficiency and require more frequent repairs after about 15 to 20 years, so it’s a good idea to consider replacement around this time to avoid higher energy bills and unexpected breakdowns. Regular maintenance can help extend the furnace's life toward the upper end of this range.
Learn More About Furnace Replacement
- Buyers Guide: 10 Things to Consider When buying a furnace
- Cost of a gas furnace
- How much does it cost to replace vs repair a furnace?
- Learn about furnace installation
- Furnace troubleshooting tips
- Discover the signs you need a new furnace
- How long does a furnace last?
- Comparing types of furnaces
- Learn the importance of furnace blower motors and signs you need a replacement
- Learn about HVAC financing and the benefits of HVAC financing