Air Purifiers for Allergies?
Indoor air quality is getting a lot of attention these days, and for good reason. According to the EPA, levels of pollutants in indoor air can be two to five times higher than outdoor air.1 Unfortunately, inside exposure to pet dander, dust mites and other airborne particulate matter can trigger allergy and asthma symptoms. That’s why it’s important to follow a simple, three-step solution to improving the quality of the air in your home.2 These steps include:
- Removing, reducing or eliminating sources of airborne pollutants
- Ventilating living areas in your home using available kitchen or bathroom exhaust fans
- Adding air filters or air purifiers to help clean the air
So, when you think about researching or purchasing air purifiers for allergies, keep in mind that while air purifiers don’t treat allergies, they can be very effective at removing allergens like pet hair and dander, pollen, and dust. It’s also important to know that the most effective solution includes taking additional steps to protect yourself.
As the indoor comfort experts, Carrier offers a number of reliable solutions for improving indoor air quality, including our Infinity® air purifiers, featuring our patented Captures & Kills® technology, that offer proven, 99% inactivation of select captured viruses and germs.3
Do Air Purifiers Help Allergies?
Answering the question, “do air purifiers help allergies?” starts with understanding how air purifiers work. In most cases, an air purifier uses a fan to circulate air into a filter or series of air filters. Depending upon the capability of the filtration system, airborne particles of various sizes are trapped, leaving cleaner, or “purified” air back into the room or home. The effectiveness of the air purifier is directly related to the capability of the filter or filters. For example, a true HEPA filter has been verified to capture 99.97 percent of airborne pollutants sized 0.3 microns in diameter.
Other air cleaning and purifying units may use electronic methods of collecting airborne particles. These units place an electrical charge on incoming particles and capture the charged particles on oppositely charged collector plates or filters. These models often include a mechanical pre-filter which must be replaced regularly. If you still have questions regarding “do air purifiers work?”, check out our web page dedicated to that topic.
According to the American College of Allergy, Asthma and Immunology, air filtration has shown an ability to reduce airborne allergens.4 Regardless of how they do it, air purifiers can help trap allergens including dust mites, pet hair, pet dander, and smoke. While avoiding these pollutants altogether is the best solution, sometimes it’s not possible. You can, however, reduce exposure to airborne pollutants in your home by:
- Banning indoor smoking
- Reducing or minimizing use of fireplaces
- Turning on exhaust fan when cooking
- Replace carpeting with hardwood floors or other hard surfaces
- Removing cloth-covered furniture and replace with leather-covered furniture
- Minimizing or removing other “soft” surfaces like decorative pillows, stuffed animals, and throws
- Cleaning all heating and air conditioner filters as required
And when you have done all that you can to eliminate sources of airborne pollutants within your home, be sure to consider the air purifier options available through Carrier. Select Carrier air purifiers have HEPA (high efficiency particulate air) filters; and, some models offer several fan speed settings which allow you to adjust for more air circulation and filtering as needed, or quieter operation if preferred. Carrier has a complete lineup of whole-home air cleaners and purifiers in addition to our newer, portable Carrier at Home air purifier.
Questions to Ask Before Purchasing an Air Purifier for Allergens
Now that we’ve discussed the benefits of air purifiers for allergies and how air purifiers can help filter out allergens, let’s take a look at some questions you should ask before making a purchase. Some examples include:
- How often will the unit clean the air in my room/home? The answer will depend upon the size of the room or home (square feet) and the air purifier’s available fan speeds.
- What substances will the air purifier clean in my home? This will depend upon the type of filter or filtration system. True HEPA filters can capture 99.97% of dust, pollen, pet dander and other particles 0.3 microns or larger. For non-HEPA filters, check for the MERV rating – the higher the number, the more effective the filter and the more types of pollutants it can capture.
- How often does the filter need to be changed? As a general rule, many air purifier filters need to be replaced once every 6 – 12 months. However, this will depend upon the type of filter and the manufacturer’s recommendations.
- What air filtration system should the air purification system have to clean your home effectively? Some of the best air purifiers on the market include technologies that can either inactivate particles trapped in the filter or combine HEPA filtration with a prefilter of some kind and / or an adsorbent filter such as activated carbon which helps remove or reduce odors.
- What is the CADR (Clean Air Delivery Rate) of the air purifier? Portable room air purifiers have a CADR rating. This is a rating that was developed by the Association of Home Appliance Manufactures (AHAM) to measure the effectiveness of an air filter based upon room space, and the volume of clean air produced per minute. CADR ratings are recorded for the three most common indoor pollutants of dust, pollen and smoke.
- What air purifier is suited for smaller rooms / bigger rooms? Portable room air purifiers often include published recommendations for appropriate room size. For example, our room air purifiers are available in two sizes, one for moderately sized rooms and one for larger rooms. Whole-home air purifiers, like the Carrier Infinity air purifier are tied into your home’s HVAC system to provide air cleaning capabilities for the entire home.
Best Air Purifiers for Allergies?
If you find yourself asking what the best air purifiers for allergies are, remember that air purifiers don’t treat allergies but instead filter out allergens that can cause allergy symptoms. You might consider air purifiers that are most effective at capturing the pollutants you and your family have sensitivities to. They also need to match your needs in terms of affordability and whether you prefer a whole-home solution or one that just focuses on one room.
As you explore your options, you should become familiar with the terminology used to compare filter quality. One such example is MERV, or Minimum Efficiency Reporting Value. MERV ratings express a whole-home air filter’s ability to capture airborne particles. Like miles-per-gallon for a car, a higher MERV number means the filter is “more efficient” - or more specifically, offers greater ability for capturing particles of a specific size. You’ll also need to pay close attention to sizing – be sure to select a purifier that is rated for the size of the room or home in which it is intended. HEPA filters or High-Efficiency Particulate Air filters are not MERV rated but rather have a 99.97% capture rate of particles sized 0.3 microns.
Carrier offers three types of air purifiers or air cleaners:
Infinity Air Purifier: The Infinity air purifier is a whole-home solution that is added to your heating and cooling system. It not only captures dirt, pollen and pet dander, it inactivates 99% of select airborne germs and viruses trapped in the MERV 15 filter -- including coronavirus, human influenza, the common cold and bacteria that causes strep throat.3 The Infinity air purifier is our most advanced solution for the entire home, and it is our highest cost option as well.
ComfortTM EZ Flex Cabinet: The EZ Flex system is not considered to be an air purifier, but rather an air filter that does provide advanced, whole-home air filtration. EZ Flex uses a deep-pleated MERV 10 filter that keeps air flowing while removing 63% of airborne particles in micron size range 1.0 to 3.0.5 They can filter common household pollutants such as dust mites, pollen, skin flakes, and other allergens. This is our most affordable whole-home solution.
Room Air Purifier: Our smart room air purifiers offer the ultimate in flexibility and effectiveness. These portable units include three levels of filtration – a pre-filter that captures larger particles such as dust, dirt and pet dander; a HEPA filter that captures up to 99.97% of particles sized 0.3 microns and an activated carbon filter for odors and VOCs. These filters can trap dust, pollen and pet dander; and an activated carbon filter that helps remove odors. While this model offers effective filtration in one area of the home, it is not considered a whole-home solution.
You can Learn more about our whole-home air purifiers and other Carrier products for your home.
1 https://www.epa.gov/report-environment/indoor-air-quality
2 https://www.epa.gov/indoor-air-quality-iaq/improving-indoor-air-quality
3 The Infinity air purifier has demonstrated effectiveness against the murine coronavirus, based on third-party testing (2020) showing a >99% inactivation, which is a virus similar to the human novel coronavirus (SARS-CoV-2) that causes COVID-19. Therefore, the Infinity air purifier can be expected to be effective against SARS-CoV-2 when used in accordance with its directions for use. Third-party testing (2012, 2007) also shows =99% inactivation for the type of virus that causes common colds, Streptococcus pyogenes and human influenza. Airborne particles must flow through your HVAC system and be trapped by the MERV 15 Infinity filter to be inactivated at 99%. The Infinity air purifier achieves a MERV 15 rating based on third-party testing (2012) showing 95% of particles size 1.0 to 3.0 microns captured and 85% of particles size 0.3 to 1.0 microns captured. Learn how it works.
4 https://acaai.org/allergies/management-treatment/living-with-allergies/air-filters/
5 Based on third party testing (2015) showing 63% of particles size 1.0 to 3.0 captured and 91% of particles size 3.0 to 10 captured.