Skip to main content
Buying Tips, Indoor Air Quality, Humidifiers

Whole House Humidifier Cost

By Travis Baugh

Buying or replacing a whole house humidifier is an investment in your home comfort. The cost depends on two factors: the type of humidifier you choose and labor for installation. The installed cost of a whole-home humidifier can range anywhere from $500 to $2,000 or more.

a man and woman research online at a desk whole house humidifier cost and whole house humidifier installation

Types of Whole Home Humidifiers

Whole house humidifiers have different price levels based on the manufacturer and the features available. Factors that impact the price of a humidifier:

  • Existing system—if you’re buying a new HVAC system or are adding a humidifier to your existing system
  • Type of humidifier—bypass, fan-powered, or steam
  • Geographic location—if you live in an arid climate, you might need a humidifier capable of producing a higher amount of water vapor per day, which can increase the cost
  • Size of home—if you live in a larger home, you might need a humidifier capable of producing a higher amount of water vapor per day, which can increase the cost
  • Warranties—warranties and extended service agreements can help reduce the overall cost of a new humidifier over time by covering maintenance and repair costs
a graphic shows different types of whole home humidifiers

Whole House Humidifier Installation

Labor can account for half of the whole house humidifier installation cost, and proper installation requires qualified technicians. Factors that affect labor costs:

  • Geographic location—labor costs vary across the United States
  • Your existing system—if the humidifier and HVAC system are both brand new or if you are adding the humidifier to an existing HVAC
  • Location of the humidifier system in your home—this impacts the amount of time it takes the technicians to complete the installation. Installing a whole home humidifier in a garage or an easy-to-access utility closet is faster than installing in an attic or crawl space.
a man discusses whole home humidifier cost with a couple

How Much Does a Whole House Humidifier Cost?

When considering the cost of humidifiers, it's important to factor in various elements. The price of a whole-home humidifier is determined by two main factors: the type of humidifier chosen and the labor involved in its installation. Depending on these factors, the installed cost can range from $500 to $2,000 or more. There are different types of whole-home humidifiers available, each with varying prices based on factors such as the manufacturer, features, existing HVAC system, geographic location, home size, and warranties. Labor costs, which can make up half of the installation cost, also vary depending on the geographic location, existing HVAC system, and the location of the humidifier system within the home. Proper installation requires skilled technicians, and the complexity of the installation location can impact the time required for the installation process.

a carrier dealer answers questions on humidifier for house cost

Connect With a Carrier Dealer To Buy A Humidifier For House

Working with a Carrier dealer to buy a humidifier for your home ensures you're getting a high-quality, reliable product tailored to your needs. Carrier dealers are experts in helping you choose the right humidifier, whether you're looking for an HVAC-integrated system or a standalone unit. They can assess your home's specific humidity levels and recommend the best option to improve air quality and comfort. Plus, with professional installation and ongoing support, you can trust that your humidifier will function efficiently, providing optimal moisture levels year-round. A Carrier dealer can also guide you through maintenance and service to keep your humidifier in top condition. Schedule an appointment with your local Carrier dealer today to get started.

Explore Carrier Whole Home Humidifiers

Consider a Carrier whole home humidifier to maintain ideal humidity levels and enhance comfort in your home. Carrier whole home humidifiers help prevent dry skin, static electricity, and respiratory issues by adding moisture to the air, especially in the winter months. They are designed for quiet operation and energy efficiency, ensuring consistent humidity control without increasing energy costs. With reliable performance and easy integration into your HVAC system, Carrier whole humidifiers promote a healthier, more comfortable living environment year-round.

Steam humidifier that can produce up to 34 gallons of water vapor per day.
Fan-powered humidifier that can produce up to 17- 18 gallons of water vapor per day.
Bypass humidifier that can produce up to 17- 18 gallons of water vapor per day.

Learn More Whole-Home Humidifiers

Chat-icon
Let's chat
- Home-icon
chat-circle-icon