Passer au contenu principal
Air Conditioners, HVAC Education, Furnaces, Heat Pumps, Maintenance

AC Refrigerant: Definition and Updates

You may not know this, but for virtually every person in modern society, refrigerant touches your life nearly every day. That cold beverage from your refrigerator... the cool breeze from your car’s air conditioning vents... and even that warm air from your heat pump... all courtesy of refrigerant.

carrier dealer checks ac refrigerant levels of ac unit

Refrigerant has been a vital part of indoor cooling systems since Willis Carrier invented the modern method of conditioning air in 1902. And chances are if you are reading this blog in the middle of summer, you are doing so in the air conditioned comfort of your home or your favorite local coffee shop.

What is AC Refrigerant? 

Refrigerant is a chemical compound capable of transitioning from liquid to gas and back again. During the process, its abilities to absorb and transfer heat have been the key to cooling, refrigeration and heat pump systems for many years.

Historically, refrigerant has been manufactured using a number of different chemical combinations. Some of the most commonly recognized names of refrigerant include:

  • Freon®
  • R-12
  • R-22
  • R-134A 
  • R-410A (Puron®)
  • R-454B (Puron Advance™)

Learn more about Puron Advance, Carrier’s new refrigerant that will replace Puron in all residential ducted and ductless and light commercial products..

chart showing different ac refrigerant classifications

What AC Refrigerant Does

Whether you call it refrigerant, Freon, R-22, R-410A, Puron or something else, it all does the same thing. As a part of your air conditioner or heat pump system, it helps transfer heat and humidity out of your home for cooling... or draws heat from outdoor air and brings it inside for heating. 

AC refrigerant plays a crucial role in the cooling process of air conditioning systems. Here’s how it works:

1) Absorbing Heat: The refrigerant circulates through the AC system in a closed loop, alternately absorbing heat from indoor air and releasing it outdoors.

2) Phase Change: As the refrigerant passes through the evaporator coil indoors, it absorbs heat from indoor air, causing it to evaporate from a liquid to a gas.

3) Compression: The compressor compresses the gas refrigerant, increasing its temperature and pressure.

4) Condensation: The hot, high-pressure gas refrigerant then flows to the condenser coil located outside or in the outdoor unit. Here, it condenses back into a liquid state, releasing the heat it absorbed from indoors to the outdoor air.

5) Expansion: The liquid refrigerant passes through an expansion valve or capillary tube, where it undergoes a pressure drop, allowing it to evaporate and absorb heat again in the indoor evaporator coil, restarting the cycle.

Learn more about how do air conditioners work.

a graphic shows how ac refrigerant passes through air conditioner

How HVAC Refrigerant Has Changed

There has been a history of change for refrigerants. The changes from R-12 to R-22 and to Puron aimed to reduce ozone depletion, while the most recent change to Puron Advance has focused on lowering GWP (global warming potential).  Below are the refrigerant implications for your heating and cooling system based on the time of install.

an infographic of ac refrigerant regulation history

What HVAC Refrigerant Means to You Now

Because air conditioning and heat pump systems can last 15 years or longer, there are still many R-22 systems in service today. 

If your HVAC system was installed in 2010 or before

  • You likely have a system with R-22 refrigerant.
  • Only “used” or “reclaimed” R-22 is available for system repairs/recharging as of 2020.

If your system was installed between 2010 and 2023

  • You probably have a system with R-410A, Puron or an equivalent, non-ozone depleting refrigerant
  • In the short-term, cost for adding refrigerant to your system should remain somewhat stable due to ample supplies
  • Due to potentially escalating costs for repairs and the phasedown of R-410A refrigerant, it may be more economically sound to replace an ailing air conditioner or heat pump with a new model that uses Puron Advance.

If your system was installed in 2024 or beyond

Puron Advance is Carrier’s new refrigerant that will replace Puron in all residential ducted, ductless, and light commercial products. This refrigerant, also known as R-454B meets the Environmental Protection Agency’s (EPA) anticipated Global Warming Potential (GWP) limits for refrigerants and the scheduled phasedown of higher GWP refrigerants like Puron™ or R-410A.
 
Effective January 1, 2025, all newly manufactured or imported HVAC indoor units, outdoor units, SPP, Mini-VRF, VRF, and light commercial products must be designed for use with a low GWP refrigerant. Puron Advance not only meets but exceeds the new requirement with a GWP of 466 and is a 75% reduction in GWP compared to R-410A.
 a

TALK TO YOUR LOCAL CARRIER DEALER FOR YOUR AC REFRIGERANT NEEDS

If your current system is struggling to keep you cool, running low on refrigerant is just one of many potential issues. The problem could be as simple as a clogged filter, or a more complicated and expensive issue with your unit’s compressor. The best way to find a solution? Contact your local Carrier HVAC contractor for professional troubleshooting, repair, or replacement with a new, higher efficiency HVAC system.

a carrier dealer explains the phase out of freon ac refrigerant to a homeowner

Trademarks are the property of their respective owners

Frequently Asked Questions About AC Refrigerant

Adding refrigerant to your home AC should be left to a professional. Improper handling can lead to system damage, safety hazards, or voided warranties. A certified HVAC technician can safely check for leaks and ensure the correct refrigerant is used.
The refrigerant used in an AC system depends on when it was installed. Systems installed in 2010 or before likely have R-22 refrigerant. Systems installed between 2010 and 2023 probably use R-410A, Puron, or an equivalent, non-ozone depleting refrigerant. If your system was installed in 2024 or beyond, it will likely use Puron Advance, also known as R-454B. Puron Advance has a low Global Warming Potential while also being non-ozone depleting.
Yes, it matters what AC refrigerant you use. Each refrigerant type has different properties, and using the wrong one can damage the system, reduce efficiency, or void warranties. It's important to use the refrigerant specified by the manufacturer.
Using the wrong AC refrigerant can damage the system, cause inefficient cooling, and increase energy consumption. It may also lead to system failure, void warranties, and potentially harm the environment due to incompatible chemicals. Always use the recommended refrigerant.
Effective January 1, 2025, all newly manufactured or imported HVAC indoor units, outdoor units, SPP, Mini-VRF, VRF, and light commercial products must be designed for use with a low GWP refrigerant, effectively banning R-454B, R-410A, R-22, and other previous refrigerants.

Learn More About AC Refrigerant

 
  • Learn about Carrier's newest refrigerant, Puron Advance™
  • Read about the history R-22 refrigerant and R-410A refrigerant