Passer au contenu principal
Air Conditioners, HVAC Education, Indoor Air Quality

What is Central Air Conditioning and How Does Central Air Work?

What is central air conditioning? How does air conditioning work in a central air system? Central air conditioning is a common term used to describe most whole-home air conditioning systems. It replaces warm air with cool air that’s been passed over cold coils, then pushes it into your living spaces. There are two different types of central air conditionerssplit systems and packaged systems. A split system has both an indoor and outdoor unit, while a packaged system is contained in a single outdoor unit to help when there is limited space.

How does a central air conditioner work?

  • When the indoor temperature rises above your desired set point, the thermostat turns on the system.
  • The fan in the indoor unit pulls warm air from inside your home into return air ducts, then passes it through filters to remove dust and airborne pollutants.
  • That air passes over the cold evaporator coil, where liquid refrigerant absorbs heat, changes it into a gas refrigerant, and cools the air.
  • The blower fan then sends the cooled air into living spaces.
  • The now-warm gas refrigerant travels to the compressor through copper tubing.
  • The compressor pressurizes the gas and sends it to the condenser coil, which releases the heat outdoors and turns the refrigerant back to liquid.
  • The refrigerant travels to the evaporator coil to continue the cycle.
a graphic shows what is central air conditioning and how does it work

Parts of a Central Air Conditioning System

  • Both a split system and a packaged system use a thermostat to control the temperature and ductwork to circulate air around the indoor living spaces
  • In a split system:
    • Outdoor unit—fan, condenser coil, and compressor
    • Indoor unit—furnace or fan coil, which houses the evaporator coil and fan to circulate cool air
    • Copper tubing—where the refrigerant flows between the indoor and outdoor units
  • In a packaged system:
    • Fan, condenser coil, compressor, and fan coil—all in one unit
a carrier central air conditioning system outside of a home

Learn More on Central Air Conditioning System Topics

Still have questions on what is central air all about? Contact a Carrier HVAC contractor to find out more about air conditioning systems and solutions. They have the knowledge and expertise to get your questions answered.

a carrier central ac dealer services a central air conditioner
How Much Does An AC Unit Cost
Learn About AC Repairs

Frequently Asked Questions About Central Air Conditioning

Air conditioner costs typically range between $3,000 - $15,000 or more. Learn more about the central air conditioner price.
The main difference between AC and central air is that "AC" typically refers to any air conditioning system, including window units or portable models, while "central air" refers to a whole-house system that cools air via ducts and a central unit.
Every unit is different and every homeowner has a different understanding of when their central air conditioner is broken beyond repair. However, with proper maintenance and care, you can expect a good 15 to 20 years of cooling from a new high efficiency air conditioning system. Learn more about air conditioner lifespan.
Adding central air to a house can be worth it if you want consistent, whole-house cooling, improved comfort, and increased home value. It’s especially beneficial in hotter climates, offering better air distribution and energy efficiency compared to window units or portable ACs.
It's generally okay for central AC to run all day if needed, especially during very hot weather. However, continuous operation can strain the system and increase cooling bills. Regular maintenance and a programmable thermostat can help optimize efficiency and prevent unnecessary wear.
Your central air conditioner may need replacement if it’s over 15-20 years old, requires frequent repairs, or no longer cools efficiently. High cooling bills, uneven cooling, and strange noises are also signs that it may be time for a replacement.
Central air conditioners should be serviced at least once a year, preferably in the spring, to ensure optimal performance. Regular maintenance includes checking the refrigerant, cleaning coils and filters, and inspecting the system for potential issues to prevent breakdowns and improve efficiency. Learn more on our AC maintenance page.

Learn More About Central Air Conditioning System Topics