Passer au contenu principal

Heat Recovery Ventilation System Guide

By Travis Baugh

In this article, we'll delve into the world of heat recovery ventilators (HRVs) and explore how a heat recovery ventilation system can significantly enhance indoor air quality and energy efficiency in your home.

a carrier dealer discusses heat recovery ventilator options with a couple interested in a heat recovery ventilation system

What is a Heat Recovery Ventilator (HRV)?

A heat recovery ventilator, also known as an HRV, is a crucial component of a well-designed HVAC system. It is a mechanical ventilation system that ensures a healthier indoor environment by exchanging stale indoor air with fresh outdoor air.

The primary function of a heat recovery ventilator is to recover heat from the exhaust air and transfer it to the incoming fresh air, thus boosting energy efficiency while maintaining proper ventilation. This is especially advantageous during colder months when opening windows for ventilation leads to significant heat loss.

Unlike an energy recovery ventilator system (ERV), which also transfers moisture content between air streams, a heat ventilation recovery system focuses mainly on heat exchange. This makes heat recovery ventilation systems particularly beneficial in climates where humidity control is less of a concern, such as northern climates.

What are the benefits of a heat recovery ventilator?

Using a heat recovery ventilator in your home offers numerous benefits. It enhances indoor air quality by removing pollutants such as allergens, dust, and volatile organic compounds (VOCs) while supplying fresh outdoor air. This is particularly vital in tightly sealed homes that lack sufficient natural ventilation.

Additionally, heat recovery ventilation systems help maintain comfortable indoor temperatures by recovering heat from the exhaust air, reducing the reliance on heating systems, which may help reduce heating and cooling bills.

Another key benefit of a heat recovery ventilation system is the balanced ventilation it provides. Balanced ventilation ensures an even exchange of indoor and outdoor air, which is crucial to help maintain neutral pressure in the home unlike an exhaust only fan that could create negative pressure.

By improving energy efficiency and reducing the need for additional heating or cooling, HRVs reduce a home’s carbon footprint as well.


How Do Heat Recovery Ventilators Work?

An heat recovery ventilator is a mechanical ventilation system that maintains a healthier indoor environment by exchanging stale indoor air with fresh outdoor air. It utilizes a sophisticated mechanism to recover heat from the outgoing stale air to pre-condition the incoming fresh air, thereby improving energy efficiency. Learn more about what is home ventilation.

The functioning of an HRV system is based on the principle of heat transfer. The unit consists of two separate air streams: one for the outgoing stale air and another for the incoming fresh air. These air streams pass through a heat recovery core made of a membrane that allows the transfer of heat between the air streams.

As the stale indoor air is expelled, it transfers its heat to the heat exchanger. Simultaneously, the fresh outdoor air passes through the opposite side of the heat exchanger, where it is preheated or precooled by the outgoing air, depending on the season.

Integrating a heat recovery ventilation system with an existing HVAC system can enhance indoor air quality and energy efficiency. Using existing ductwork, the heat recovery ventilator can exchange stale, polluted air with fresh outdoor air while recovering heat from outgoing air to pre-condition incoming air.

Proper placement of the heat recovery ventilator is essential for optimal performance, ensuring balanced air exchange throughout the home. Regular cleaning and filter replacement are necessary to maintain the system's efficiency and prevent dust and pollutant buildup.

Heat Recovery Ventilation Systems and Energy Efficiency

Heat recovery ventilators are an excellent way to improve energy efficiency in homes. Heat recovery ventilation systems recover and reuse heat that would otherwise be lost during ventilation, helping to reduce energy waste and lower heating and cooling bills.

By extracting heat from outgoing stale air and transferring it to incoming fresh air, heat recovery ventilation systems ensure that the energy used to heat or cool indoor air is not wasted. This process leads to significant energy savings, as conditioned air retains much of its temperature when reintroduced into the living space.

One of the key benefits of heat recovery ventilation systems is their ability to reduce heating and cooling costs. By recovering heat from exhaust air, heat recovery ventilation systems decrease the energy required to heat incoming fresh air during winter. Similarly, during summer, the system helps pre-cool incoming air, reducing reliance on air conditioning. This results in lower energy consumption and substantial savings on heating and cooling bills.

a woman relaxes on the couch in a home with a carrier heat recovery ventilation system installed

Heat Recovery Ventilator (HRV) Maintenance

Proper maintenance of a whole-home heat recovery ventilator (HRV) is essential for maintaining indoor air quality, energy efficiency, and system longevity. Regular maintenance ensures optimal performance and prevents airflow blockages, excess humidity, and potential mechanical failures.
 a carrier dealer explains heating recovery ventilator options to a couple

Key Maintenance Tasks

  • Clean or Replace Filters – HRV filters capture dust, pollen, and debris. Clean them every 1-3 months and replace them as needed to maintain efficient airflow.
  • Inspect and Clean the Core – The heat exchange core should be cleaned every 6-12 months with warm water or a vacuum to remove accumulated dirt.
  • Check and Clean Vents & Ducts – Ensure that both indoor and outdoor vents are free from blockages like leaves, dust, or ice buildup. Clean ductwork periodically to maintain proper air circulation.
  • Inspect the Drainage System – If your HRV has a condensate drain, check for clogs and clean it to prevent water buildup.
  • Test the Fans and Motors – Ensure fans run smoothly and listen for unusual noises that may indicate wear or damage.
Routine HRV maintenance improves efficiency, extends the unit’s lifespan, and ensures a consistent supply of fresh, filtered air in your home.

Connect With Your Carrier Dealer On Heat Recovery Ventilation Systems

At Carrier, we understand the importance of proper ventilation in your home. Our range of ventilation systems are designed to provide improved indoor air quality while maximizing energy savings. Incorporating advanced technology and key features, our heat recovery ventilators offer a reliable and efficient solution for your ventilation needs.

Choosing the right heat recovery ventilation system is crucial for ensuring a healthier and comfortable indoor environment. Connect with your local Carrier dealer to find the right heat recovery ventilator for your home. Working with your Carrier dealer on a heat recovery ventilator (HRV) ensures you get expert guidance on selecting, installing, and maintaining the right system for your home. Carrier dealers are trained to optimize HRV performance for maximum energy efficiency, air quality, and comfort. Plus, they provide professional service, warranty support, and routine maintenance to keep your system running smoothly for years to come. Schedule an appointment with your local Carrier dealer today.

a graphic explains different types of heat recovery ventilators

Frequently Asked Questions About Heat Recovery Ventilators

A Heat Recovery Ventilator (HRV) is a system that improves indoor air quality and energy efficiency by exchanging stale indoor air with fresh outdoor air.
A heat recovery ventilators recovers heat from the outgoing air to precondition the incoming air, helping reduce heating and cooling demands.
Heat Recovery Ventilators (HRVs) transfer heat between outgoing and incoming air, improving temperature control without affecting humidity. They are ideal for climates with extreme temperatures but moderate humidity. Energy Recovery Ventilators (ERVs) transfer both heat and moisture, balancing indoor humidity levels in addition to temperature. ERVs are best for climates with high humidity. Both systems improve indoor air quality and energy efficiency, but ERVs provide added humidity control.
Ventilation heat recovery systems can be highly effective in recovering heat. According to Science Direct, HRV systems can recover 60-95% of the heat from outgoing air, significantly reducing heating and cooling costs.1
A Heat Recovery Ventilator (HRV) may be worth it if you are looking to improve indoor air quality and energy efficiency. HRVs help reduce heating and cooling costs by recovering the heat from outgoing air, providing fresh air without significant energy loss. HRVs help maintain consistent indoor temperatures and enhance comfort, making them a valuable investment for better air quality.
You can run a Heat Recovery Ventilator (HRV) continuously to maintain optimal indoor air quality and energy efficiency. However, depending on the product and controls installed you can adjust the settings to only run during occupancy, which increases airflow when the house is occupied or during activities that generate moisture such as cooking or showering.
 
The lifespan of an HRV system is typically 10 to 15 years, with proper maintenance. Regular filter changes and system checks can help extend its efficiency and longevity.
 
The cost to install a Heat Recovery Ventilation (HRV) system typically ranges from $2,000 to $5,000, depending on factors like home size, complexity of the installation, and system brand. For retrofits, costs can be higher due to ductwork modifications. Talk to your local Carrier dealer for an accurate quote for an HRV for your home.
No, a heat recovery ventilation (HRV) system cannot cool a house. It only exchanges heat between incoming and outgoing air, helping to maintain temperature balance. For cooling, an air conditioning system is required.
 
It's generally recommended to run your HRV system continuously for optimal air quality and energy efficiency. However, you can adjust the settings based on your needs, such as during high occupancy or specific ventilation requirements.
 
No, an HRV system does not dehumidify the air in summer. It only exchanges air while recovering heat, but it does not control humidity. For dehumidification, a separate system, like a whole-home dehumidifier, is needed.
HRV systems can be expensive to install, especially for retrofit application. Regular cleaning and upkeep are required to maintain efficiency. HRVs may have reduced efficiency in very cold or very hot climates.

Explore Carrier Heat Recovery Ventilators

A Carrier heat recovery ventilator (HRV) enhances indoor air quality by efficiently exchanging stale indoor air with fresh outdoor air, while retaining energy. It helps maintain optimal humidity and temperature levels throughout the year, promoting a healthier and more comfortable living environment. By reducing the need for excessive heating or cooling, an HRV also contributes to energy savings, making it an eco-friendly choice for homeowners. Explore Carrier's line of heat recovery ventilators today.

Idéal pour les climats nordiques et les installations horizontales. Offre un débit d’air jusqu’à 3 m3/min (231 pi3/min). La couleur de la porte passe lentement de « havane » à « acier galvanisé ».*

Idéal pour les climats nordiques et les installations horizontales. Offre un débit d’air jusqu’à jusqu’à 4,53 m3/min (160 pi3/min).

Ideal for northern climates and vertical installations. Offers airflow up to 160 cubic feet per minute