Carrier Transicold Expands Supra HE Range with Two New Multi-Temperature Units
RUEIL-MALMAISON, France -
Carrier Transicold is expanding its line of Supra® High Efficiency (HE) truck-mounted refrigeration units with the launch of the Supra HE 11 Multi-Temperature (MT) and HE 13 MT. These two high-performance, compact and fuel-efficient systems are designed for compatibility with one of the most comprehensive ranges of evaporators on the market. Carrier Transicold is part of Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions.
Available in standard and silent versions, the Supra HE 11 MT and HE 13 MT units are designed to meet a wide range of refrigerated transport needs, supporting various configurations, including double compartment setup for the Supra HE 11 and the option of either double or triple-compartment setup for the Supra HE 13 MT. Based on the dimensions of the box and the specific application requirements, the Supra HE 11 MT and HE 13 MT units provide two distinct levels of cooling capacity, the latter being the most powerful of the range. Additionally, Carrier Transicold has increased evaporator airflow capacity by up to 32% compared to the legacy Supra remote evaporators to enhance air circulation and ensure consistent temperatures throughout the vehicle’s interior.
The Supra HE MT delivers enhanced performance with improved cooling power and reduced fuel consumption. Rigorously tested in extreme conditions ranging from minus 30 degrees C to 55 degrees C, the system provides reliable operation in any environment.
Its updated lightweight, compact design allows for seamless adoption into a variety of vehicle body types while maintaining cab tilting capability for easy maintenance and accessibility.
“Carrier Transicold is setting new efficiency standards in multi-temperature refrigerated transport with the Supra HE 11 MT and HE 13 MT units,” said Jean-Michel Vadecard, Product Director Truck Trailer International, Carrier Transicold. “These solutions deliver optimized refrigeration performance, reduced fuel consumption, a compact design and enhanced airflow capabilities to accommodate all rigid truck configurations on the market.”
Each unit in the Supra HE line comes equipped with telematics hardware and is compatible with Carrier Transicold’s Lynx Fleet digital platform.
For more information about Carrier Transicold products and services, visit Carrier Transicold.
About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, global leader in intelligent climate and energy solutions, committed to creating innovations that bring comfort, safety and sustainability to life. For more information, visit www.carriertransicold.eu. Follow Carrier Refrigeration on X: @SmartColdChain and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.