Carrier Transicold’s X4 7700 Trailer Refrigeration Unit Now Available
Ga., ATHENS -
Boasting high refrigeration capacities, demonstrated fuel savings of 20-25% and reduced emissions for greater sustainability and regulatory compliance, Carrier Transicold’s new X4™ 7700 trailer refrigeration unit is now available through the company’s North America dealer network. Carrier Transicold is a part of Carrier Global Corporation (NYSE: CARR), the leading global provider of healthy, safe, sustainable and intelligent building and cold chain solutions.
“In full production at our world-class manufacturing facility in Athens, Georgia, the new premium performance X4 7700 single-temperature unit builds on the X4 platform’s decade-long reputation for high capacity and rugged, dependable service,” said Bill Maddox, Senior Manager of Product Management, Truck Trailer Americas, Carrier Transicold. “Continuing the tradition of reliable design and simply smarter engineering, the X4 7700 unit offers a 96% reduction in particulate emissions and double-digit gains in fuel efficiency compared to standard X4 models.”
The new unit employs an advanced version of the smart engine used throughout Carrier Transicold’s existing trailer platforms. Benefits of the new unit include:
- Enhanced compliance – Under current regulations, the X4 7700 provides lifetime compliance with the California Air Resources Board’s (CARB) stricter rules for trailer refrigeration systems.
- Significantly better fuel economy – The advanced engine features common-rail fuel injection for optimized fuel delivery that reduces fuel consumption by 5-10%. The new third speed called “eco speed” automatically decreases engine RPMs during intervals where conditions permit, significantly improving operating efficiency compared to normal low-speed operation for even more fuel savings. Combined, these performance enhancements demonstrated 20 to 25% average fuel savings, relative to standard X4 units, for premium performance X4 7700 units tested by over-the-road fleets under a variety of operating conditions during the summer of 2022.
- Greater sustainability – The unit uses R-452A refrigerant with a global warming potential 45% lower than that of the traditional transport refrigeration unit refrigerant, R-404A. The efficient common rail fuel system and a diesel oxidation catalyst push particulate, hydrocarbon and NOx emissions to new lows, and the unit is the most environmentally responsible choice in the X4 Series for fleets seeking sustainable options.
- Lighter weight – At 1,690 pounds, the X4 7700 weighs about 10% less than its competition.
- Highest capacity – As with its predecessor in the X4 Series, the X4 7700 achieves the high industry benchmark of 68,000 BTU/h at a setpoint of 35 degrees Fahrenheit under certification conditions of the Air-Conditioning, Heating & Refrigeration Institute.
“The X4 7700 provides more BTUs of cooling per engine RPM than competitive units, meaning competitive units must run harder than an X4 unit to achieve similar results,” Maddox said.
All X4 7700 units are equipped with Carrier Transicold’s industry-leading LynxTM Fleet telematics solution for remote monitoring of temperatures, location, movement and system operating performance. To help maintain the charge of the battery supporting the unit and its telematics system, Carrier Transicold now also offers its TRU-Mount solar panel as a factory-installed option.
Carrier Transicold’s CARB-compliant TRUs help fleets significantly reduce their environmental impact, supporting Carrier’s 2030 Environmental, Social and Governance Goal of reducing its customers’ carbon footprint by one gigaton.
For more information about the X4 7700 trailer refrigeration unit, turn to the experts in Carrier Transicold’s North America dealer network.
About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, the leading global provider of healthy, safe, sustainable and intelligent building and cold chain solutions. For more information, visit Carrier Transicold. Follow Carrier on Twitter: @SmartColdChain, on Facebook at Carrier Transicold Truck/Trailer U.S. & Canada and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.
![](https://images.carriercms.com/image/upload/w_auto,c_limit,dpr_auto,f_auto/v1677613257/carrier/carrier-global/news/news-article/2023/Carrier-Transicold-X4-7700-Trailer-Refrigeration-Unit-6x9.jpg)