What is A Split Air Conditioner? Your Guide To Split AC Units
How does air conditioning work as a split HVAC system? A split HVAC system is an air conditioning system or heating system that has both indoor and outdoor units that are connected with copper tubing.
Traditionally, the outdoor portion of the unit contains the compressor and condenser, and the indoor portion of the unit contains an evaporator coil and indoor air handling unit that sends the air through the ductwork in your home. These types of home cooling systems are different from HVAC packaged units, where all parts are packaged together in one unit.
There are many different types of split systems, which can include heat pump systems or air conditioning systems (larger homes might require multiple split system air conditioners) installed outside your home, paired with either a gas furnace or a fan coil located inside your home.
5 Different Types of Split System Cooling and Heating Systems

1. Split System Heat Pumps
Heat pumps run on electricity and draw heat from outside air—even cold air—and transfer it indoors. The outdoor unit houses a compressor and heat exchanger, and the indoor unit has an air handler and fan that circulate the air inside the home.
2. Split System Air Conditioners
Split-system air conditioners are units with the condenser and compressor placed outdoors, and an indoor unit containing the evaporator, furnace, air handler, and filters.

3. Furnaces
Furnaces are indoor units that burn fuel, like gas or propane, to heat up the air, then distribute it through ductwork in your home.
4. Fan coils
Fan coils are indoor units that move air over the coil, heat or cool it depending on the weather and season, then distribute it through ductwork in your home.
5. Ductless vs. Ducted Systems
Split-system HVAC can be ducted or ductless. Ducted split systems use ductwork to circulate the warm air generated from your furnace, fan coil, or heat pump, and the cool air generated by your air conditioner, heat pump, or fan coil. Ductless mini split systems use small air handlers located in specific areas in your home to heat or cool that individual space.
What Is A Split Air Conditioner's Benefit?
Split HVAC systems have many benefits compared to HVAC packaged units. However, it is important to keep in mind that different types of ducted air conditioners and mini split air conditioners have benefits for different types of homes, apartments, and condos. While one HVAC system might be best suited for one type of home, it may not be best for another. Our dedicated team of Carrier experts can help you determine the best type of split HVAC system for your home and budget.
Efficiency
The efficiency ratings for HVAC split systems can range from the minimum efficiency allowed by the Department of Energy (DOE), to high-efficiency systems with ratings up to 24 SEER2. Split systems that are Energy Star® certified are considered much more energy efficient than those that rated the DOE minimum efficiency standards. Having a more energy-efficient unit can help you to save money on heating and cooling costs, which are traditionally the most expensive parts of your energy bill.
Customization
HVAC split systems have two separate components, which allows for more customization in the setup of the system.
Out of Pocket Savings
What Is A Split AC Unit Downside?

More Expensive Installation
Since there are two separate units that comprise the system, split HVAC systems tend to be more expensive to install compared to HVAC packaged units. The installation costs can also increase if the two separate units have to be installed farther apart. The installation costs can vary widely for different types of HVAC split systems, and ductless systems can have more expensive units, but don’t require any air ducts to be installed in your home.
Outside Noise
If the outdoor split AC is not properly maintained, the unit can be pretty noisy, which can hinder your experience in your yard or on your patio. This can also cause problems if you’re a light sleeper and the split system air conditioner is placed close to a bedroom.
The Outdoor Unit Requires Space
Since part of the system lives outdoors, there is space needed for the outdoor split air conditioner. This makes it difficult to install these systems if you have a small yard or outdoor space.
Contact an HVAC Expert About Split AC Units and Split Air Conditioners
Our dedicated team of HVAC professionals can help you to determine the best type of HVAC system for your home and can properly install your new split air conditioner in your home. Find a dealer near you to get started on your new HVAC split system today!
Frequently Asked Questions About Split System Cooling Units
Explore Carrier Split Air Conditioners
Carrier air conditioners are known for their reliability, energy efficiency, and advanced technology. With a range of models to suit different needs, Carrier offers solutions with optimal comfort and air quality. Whether you're looking for a budget-friendly option or a high-end, energy-efficient unit, Carrier’s air conditioners provide consistent performance, quiet operation, and innovative features.
Up to 21 SEER2 for premium energy savings with premium comfort features
Up to 16.5 SEER2 for enhanced energy savings with standard comfort features.
Learn More About Split Unit Air Conditioners
- Learn How to Change Air Conditioner Filters
- Discover the factors of Central Air Conditioner Prices
- Learn about Air Conditioner Filters
- AC maintenance and Air Conditioner Service
- HVAC meaning: What is HVAC?
- Find Out How Do Air Conditioners Work
- Learn about air conditioner installation
- Wondering “What Size Air Conditioner Do I Need?”
- How Long Do Air Conditioners Last?
- Air Conditioner Maintenance tips
- Best temperature for AC - What air conditioner temperature you should set your thermostat to.
- Troubleshoot an Air Conditioner tips
- Learn about Air Conditioner Coil Cleaning
- Tips to Unclog Air Conditioner Drain Line
- How Often to Change AC Filter
- Why is my AC Fan Not Working?
- Is your Air Conditioner Not Cooling?
- Why you should get an AC Tune Up
- Discover the benefits of UV lights for air conditioners