Skip to main content

Why Is My Air Conditioner Blowing Hot Air? Tips to Troubleshoot and Fix

By Travis Baugh

Discovering that your air conditioner is blowing hot air instead of providing the cool comfort you need can be frustrating. This issue can arise from several potential causes. Understanding the causes can help you troubleshoot and fix the problem efficiently. In this article, we'll delve into the common reasons behind an AC blowing warm air and offer practical solutions to restore its cooling performance.

a carrier dealer inspects air conditioner blowing hot air

How Does An AC Work?

An air conditioner (AC) works by using a series of components to cool the air and maintain a comfortable temperature. The compressor pumps refrigerant through the system, where it is compressed and turned into a high-pressure gas. The gas then flows through the condenser coils, releasing heat and cooling down. The refrigerant moves to the expansion valve, where it turns into a low-pressure liquid. It then passes through the evaporator coils, where it absorbs heat from the indoor air, cooling it down. The cool air is circulated by the blower fan while the refrigerant returns to the compressor to repeat the cycle. Learn more about how air conditioners work.

Six Possible Reasons For An Air Conditioner Blowing Warm Air

When your air conditioner is blowing hot air, identifying the root cause is crucial. Here are some common reasons that might explain why your AC isn't cooling your home as it should.

1. Dirty air filters

Dirty air filters are one of the most frequent culprits if your AC is running but not cooling . When dust and debris accumulate in the filters, airflow is obstructed, reducing the unit's cooling capacity. Regularly replacing air filters can help maintain proper airflow and prevent hot air from being circulated. Learn more about how to change air filters and how often to change air filters.

2. Refrigerant leak

AC refrigerant is essential for cooling the air by absorbing heat from indoors. A leak in the refrigerant lines can result in insufficient refrigerant, causing the system to blow hot air. A professional HVAC technician can locate and repair the leak, then recharge the system with the correct amount of refrigerant.

3. Thermostat issues

A malfunctioning thermostat can also lead to your AC blowing hot air. If the thermostat isn't accurately sensing the temperature or is set incorrectly, it may not send the right signals to the cooling system. Checking the thermostat settings, replacing batteries, or recalibrating the thermostat can help resolve this issue.

4. Electrical Problems

Issues with electrical components, such as contactors or capacitors, can affect cooling performance.

5. Blower Motor Issues

If the blower motor isn’t working properly, it might not circulate cool air effectively.

6. Compressor Problems

The compressor  is essential for cooling; if it fails, the system may blow hot air.
 
graphic shows inside of air conditioner and causes of AC blowing hot air

How to Troubleshoot Air Conditioner Blowing Hot Air

Before calling a professional, try these troubleshooting steps to get your AC back to blowing cool air:
  1. Check air filters and clean or replace if necessary. Clogged or dirty air filters can restrict airflow and cause your air conditioner to blow hot air. Regularly check your filters and clean or replace them as needed. This simple step often resolves the issue.
  2. Ensure thermostat settings are correct. Sometimes, the problem may lie with the thermostat settings. Ensure your thermostat is set to the desired temperature and mode. Also, check if the batteries need to be replaced.
  3. Verify the power supply. Ensure the circuit breaker for the AC unit is not tripped. Reset it if needed. Make sure the power switch to the AC unit is turned on.
  4. Check the condenser coils. Over time, these coils can accumulate dirt and debris, hindering the cooling process. Turn off the power to your air conditioner and gently remove visible dirt or debris using a soft brush or vacuum cleaner. Be careful not to bend or damage the delicate fins on the coils. Learn more about air conditioner coil cleaning .
  5. Check and clean the evaporator coils inside the air handler unit. Dirty or clogged evaporator coils can prevent your AC from cooling properly. Remove the access panel and use a soft brush or cloth to gently remove dirt or dust. A mild detergent and water solution can be used for stubborn dirt. Learn more about how to clean evaporator coils .
  6. Lastly, inspect and clean the outdoor unit. Debris, leaves, and grass clippings can accumulate around the unit, obstructing airflow. Turn off the unit and remove any debris using a brush or hose.
If these troubleshooting steps don't resolve the issue, it's recommended to contact a professional HVAC technician. 

Preventing AC from Blowing Hot Air in the Future

To prevent your air conditioner from blowing warm air, regular AC maintenance is key. Start by replacing the air filters every 1-3 months to ensure proper airflow and prevent the system from overworking. Cleaning the coils and ensuring the drain lines are clear can prevent debris buildup that could hinder cooling.
 
It’s important to schedule professional AC inspections with your local Carrier dealer at least once a year. An experienced technician will check refrigerant levels, inspect the compressor and condenser, and ensure the system is operating efficiently.
 
To optimize performance, seal gaps around windows and doors to keep cool air inside, and use ceiling fans to help circulate the cool air more evenly. Setting the thermostat at a consistent temperature can also prevent the system from unnecessary strain. Regular maintenance and professional care can extend your AC’s lifespan and keep it blowing cool air when you need it most.

Carrier Dealers Can Help With Air Conditioners Blowing Warm Air

At Carrier, we understand the importance of a properly functioning air conditioner. Our network of Carrier dealers is trained to diagnose and fix a wide range of AC issues. With their expertise, they can help restore your AC's performance and keep your home cool and comfortable. Contact your local Carrier dealer  today to schedule a service appointment.
a homeowner asks a carrier dealer why is my ac blowing hot air

FAQs About Air Conditioners Blowing Hot Air

Yes, you should turn off the AC if it is blowing warm air. Continuing to run the system could lead to further damage or inefficiency. Turning it off allows you to avoid potential harm to the compressor or other components, safely inspect or address common issues like thermostat settings, air filters, or ductwork problems, and save on energy costs while the system is not functioning properly.
A few steps you can take to fix your AC include ensuring the thermostat is set to “cool” and lower than room temperature, replacing the air filter if dirty, cleaning the condenser coil if dirty, and verifying the power supply is running to the unit.
The cost to fix an AC blowing hot air typically ranges from $150 to $600, depending on the issue. Common repairs, such as replacing a thermostat, fixing a refrigerant leak, or repairing a compressor, can vary in price. Your local Carrier dealer can provide a more accurate estimate based on the problem.
If your AC is blowing hot air, it could indicate several issues, such as low refrigerant levels, a dirty air filter, a broken compressor, or a thermostat malfunction. These problems prevent the system from cooling effectively and may require professional inspection and repair.

LEARN MORE ABOUT AIR CONDITIONER ISSUES

Chat-icon
Let's chat
- Home-icon
chat-circle-icon