Skip to main content

Your Guide To Electronic Air Cleaners

Concerned about your home's air quality? An electronic air cleaner could be the solution you need. These advanced devices improve the air you breathe by eliminating pollutants and allergens. 
 
But how do electronic air cleaners work, and what sets them apart from other air purifiers? In this guide, we'll delve into the mechanics of electronic air cleaners, highlight their benefits, and provide tips for selecting the ideal model for your home.
a carrier dealer discusses electronic air cleaners with homeowners

How Does an Electronic Air Cleaner Work?

Electronic air cleaners are highly effective in enhancing indoor air quality by capturing airborne pollutants. 
 
Electronic air cleaners operate on the principle of electrostatic attraction. They use ionization to charge airborne particles like dust, pollen, pet dander, and smoke. These charged particles are then drawn to oppositely charged collection plates inside the air cleaner.
 
Key components of electronic air cleaners include:
  • Pre-filter: Captures larger particles and extends the life of the electronic cell.
  • Electronic cell: The core of the air cleaner, containing ionizing wires and collection plates to capture charged particles.
  • Fan: Circulates air through the cleaner for effective filtration.
  • Control panel: Allows you to adjust settings, monitor air quality, and set maintenance reminders.

Benefits of Using Electronic Air Cleaners

Electronic air cleaners offer several advantages:
  • Enhanced air quality: They help reduce allergens, asthma triggers, and respiratory irritants.
  • High filtration efficiency: They capture a wide range of pollutants, including dust, pollen, pet dander, mold spores, and even bacteria and viruses
  • Low maintenance: Washable collection plates and replaceable pre-filters make upkeep easy.
  • Energy efficiency: They do not hinder HVAC system performance, unlike traditional filters.

Choosing the Right Electronic Air Cleaner

Investing in an electronic air cleaner can greatly improve your indoor air quality. However, with many options available, it's crucial to choose the right one for your needs. Consider these key factors:
  1. Size Matters: The size of the air cleaner is vital for its effectiveness. A unit too small won't adequately clean the air, while an overly large one may be costly and take up too much space. Match the cleaner's capacity to the square footage of the area you want to purify.
  2. Filtration Efficiency: The filtration efficiency is essential when selecting an air cleaner. Check the Minimum Efficiency Reporting Value (MERV) rating, which indicates the filter's ability to remove particles. Higher MERV ratings mean better filtration, but they may also require more frequent filter replacements. 
  3. Maintenance Requirements: Different models have varying maintenance needs. Some require regular cleaning, while others need filter replacements at set intervals. Consider your willingness and availability to perform maintenance tasks. Also, ensure that replacement filters are readily available for the model you choose.

Infinity Air Purifier

When choosing an electronic air cleaner, it's essential to go with a reliable brand like Carrier. Our Infinity Air Purifier delivers superior performance and efficiency, ensuring cleaner air for you and your loved ones. It is engineered to capture and filter particles as small as 0.3 microns, including allergens, dust, and pet dander. This air purifier can inactivate 99% of select airborne pathogens trapped by its MERV 15 filter, including coronavirus, bacteria, the common cold, human influenza, and other pathogens. This whole-home filtration system works silently in-line with your HVAC system to help reduce pet dander, pollen, dirt and other particles that can circulate throughout your home. 
 
Its patented Captures & Kills technology traps 95% of particles in micron size range 1.0 to 3.0 flowing through the HVAC system and subjects them to an intense electric field. The Infinity Air Purifier is available in various sizes that can accommodate most homes. Schedule an appointment with your local Carrier dealer to get one installed today.

Frequently Asked Questions About Electronic Air Cleaners

Electronic air cleaners require regular maintenance:
1. Cleaning: Clean the ionizing wires or collection plates according to manufacturer guidelines to remove accumulated particles.
2. Filter Replacement: Replace any pre-filters as recommended to prevent debris buildup and maintain airflow.
3. Inspection: Periodically check for damage or wear on components like wires and filters.
4. Power Supply: Ensure the power supply is functioning correctly and replace if necessary. 
Electronic air cleaners can last 10-20 years with proper maintenance. Regular cleaning of the plates or filters is crucial to ensure optimal performance and longevity. The lifespan also depends on usage and environmental factors, such as air quality and the presence of pollutants.
Yes, electronic air cleaners work by using electrically charged plates or filters to capture airborne particles such as dust, pollen, and smoke. They are effective at improving indoor air quality, especially for small particles. While they reduce airborne contaminants, they may not eliminate all allergens or pathogens, so they are best used in conjunction with other air quality strategies.  Remember that HVAC fans must be operating for the filters to clean the air.
carrier dealer discusses best air purifier for home with homeowner

Learn More About Air Purifiers

Chat-icon
Let's chat
- Home-icon
chat-circle-icon