What Is a Mini Split Air Conditioner?
A mini split air conditioner (often called a ductless mini split) is a ductless heating and cooling system offered by Carrier and other HVAC manufacturers that allows you to control the temperature in individual rooms or spaces. Unlike traditional central air systems that require ductwork, mini splits consist of two main components: an outdoor compressor/condenser and an indoor air-handling unit. They are linked by a conduit housing the power cable, refrigerant tubing, and condensate drain line, where required.
Whether you are updating an older home without ductwork, building a new addition, or simply want more precise control over your home's climate, choosing a mini split offers a versatile, energy-efficient solution. By eliminating the need for ducts, these systems avoid energy loss associated with ductwork, potentially lowering your energy bills while improving comfort.
What Is a Mini Split Air Conditioner?
A Carrier ductless mini split can provide targeted heating and cooling without requiring a traditional duct system. Depending on the system and configuration, Carrier mini splits can serve individual rooms or multiple zones throughout a home.
Mini Split Air Conditioner At A Glance
| Feature | Typical Mini Split Considerations |
| Efficiency | SEER2 and HSPF2 ratings vary by Carrier system and model. Carrier offers SEER2 up to 35.1 and HSPF2 up to 30 with the 37MPRA. |
| Zones | Single-zone systems connect one indoor unit to one outdoor unit; multi-zone systems can connect multiple indoor units to one outdoor unit, depending on the system. |
| Indoor sound | Sound levels vary by indoor unit and operating mode; some Carrier ductless indoor units operate at sound levels as low as the low 20s dB. |
| Refrigerant lines | Maximum line-set length varies by Carrier model and system configuration. |
| Heating performance | Carrier ductless heat pump operating ranges vary by model and outdoor temperature. |
Always check the specific Carrier product specifications for exact efficiency, sound, capacity, operating temperature and line-set limits.
How does a mini split work?
Ductless air conditioners utilize the same cooling cycle as a typical central air conditioning system but deliver the air differently. Instead of pushing air through a centralized network of ducts, a mini split circulates refrigerant between the outdoor unit and an indoor unit installed directly in the living space.
Here is the basic process:
- Heat Absorption: The indoor unit’s coil absorbs heat and humidity from the room.
- Refrigerant Transport: The heat is transferred via refrigerant to the outdoor compressor.
- Heat Release: The outdoor unit releases the heat energy into the outside air.
- Cool Air Return: The cooled refrigerant cycles back to the indoor unit, blowing crisp, cool air into your room.
Carrier ductless systems use this same basic refrigeration cycle, with inverter-driven technology adjusting compressor operation based on the heating or cooling demand.
A ductless mini split heat pump operates the same way but can reverse this process to provide efficient heating during colder months.
Clint Newsome, owner of Albany Air Conditioning and Heating Co. in Albany, GA explains that ductless mini split systems provide heating and cooling without the need for traditional ductwork, making them a flexible and energy-efficient option for many homes.
“Unlike a conventional HVAC system that relies on ductwork in an attic or crawl space, a ductless system uses individual indoor units mounted on a wall or ceiling to condition specific areas of the home,” Newsome said. “Each indoor unit operates with its own thermostat, allowing homeowners to control the temperature in that particular space. Depending on the setup, a system can include either a single outdoor condenser connected to one indoor unit or multiple indoor air handlers connected to the same condenser.”
Versatile Installation Options
One of the defining features of what is a ductless ac is its flexibility. Indoor units can be installed in various configurations:
- Wall Mounted Air Conditioners: The most common style, mounted high on an interior wall.
- Floor Consoles: Ideal for rooms with low ceilings or slanted walls.
- Cassette Units: Mounted flush into the ceiling for a streamlined look.
- In-Ceiling Units: Hidden from view if ceiling space allows.
Single- and Multi-Zone Mini Split AC Systems
When asking "what is a mini split ac," it is crucial to understand zoning. Mini splits can be configured as single-zone or multi-zone systems, offering you the ultimate HVAC flexibility for renovations, sunrooms, or older homes.
Single-Zone Ductless Air Conditioners
A single-zone system consists of one outdoor unit connected to one indoor unit. This setup is perfect for cooling a specific area, such as a garage, a new room addition, or a server room.
Multi-Zone Ductless Air Conditioners
A multi-zone system connects a single outdoor compressor to up to five indoor units. Each indoor unit is controlled independently, allowing you to set different temperatures for different rooms. Learn more about single-zone vs multi-zone ductless mini split systems.
You can even expand your system over time. For example, you might start with two indoor units and add more later as your budget or renovation needs change. Explore options for 3 zone mini splits and 4 zone mini splits.
What is the benefit of a ductless AC system?
Homeowners choose Carrier ductless air conditioner systems for their efficiency, quiet operation, and ease of installation.
- Minimal Installation: No ducts means no major construction. Installation typically requires just a small three-inch hole in the wall for the conduit. Learn more about installing a mini split.
- Energy Efficiency: Traditional ducts can lose up to 30% of energy. Mini splits eliminate this loss. Additionally, inverter-driven compressors adjust speed to match the heating or cooling load, avoiding inefficient on/off cycling. Learn about mini split efficiency.
- Precise Comfort Control: Stop fighting over the thermostat. Each zone can be set to a different temperature, so your bedroom can be cool while the living room stays warm.
- Quiet Operation: Ductless systems are quiet. The noisy compressor is outside, and long refrigerant lines allow you to place it far away from patios or bedrooms.
- Improved Air Quality: With filtration at every indoor unit, dust and allergens are trapped before air is recirculated, reducing cross-contamination between rooms.
Newsome added that many homeowners choose ductless systems because of their strong energy efficiency and lower operating costs.
“Most of the ductless systems we install are ENERGY STAR certified and designed to operate very efficiently year-round,” he said. “They typically cost very little to run and are built for continuous operation. On the heating side, many ductless heat pump systems can provide efficient heating without relying heavily on electric resistance heat, which can help reduce winter energy costs during colder weather. Overall, they’re considered a very economical solution for many homeowners.”
Pros and Cons of a Ductless Air Conditioner
Pros | Cons
|
Highly efficient cooling and heating (high SEER ratings).
| Upfront installation cost can be higher than traditional systems.
|
Easy installation with no painting or patching required.
| Aesthetics: Indoor units are visible on the wall (though sleek designs exist).
|
Zoned comfort ensures every room is the perfect temperature.
| Maintenance: Filters require regular cleaning to maintain performance.
|
Versatile solution for garages, basements, and attics.
| Whole-home limitations: Extremely large homes may need multiple outdoor units.
|
Learn more about mini spit pros and cons.
Carrier Ductless Mini Split Options
Carrier offers a range of ductless mini split systems designed to provide flexible heating and cooling for individual rooms, specific zones, or multiple areas throughout the home. With different system configurations, indoor unit styles, and efficiency options available, Carrier ductless mini splits can be tailored to a variety of home comfort needs.
| Carrier Model | Zones Supported | Cooling Efficiency | Heating Efficiency | Sound level |
| Infinity 35 37MPRA | One | Up to 35.1 SEER2 | Up to 30 HSPF2 | As low as 57 decibels |
| Infinity® 25 37MGHA | Up to five | Up to 25 SEER2 | Up to 11.3 HSPF2 | As low as 61 decibels |
| Performance 25 37MGRA | Up to six | Up to 25 SEER | Up to 10.4 HSPF2 | As low as 59.5 decibels |
Connect with a Carrier dealer
Ready to experience the future of home comfort? Find a local Carrier dealer to get a quote and see which ductless mini split air conditioner is right for your home..
Frequently Asked Questions
A mini split system (or ductless mini split) is an HVAC system with an outdoor unit and one or more indoor units that heat and cool individual rooms without ductwork. It offers precise zoning and high energy efficiency.
The main difference is ductwork. A central air conditioner uses ducts to distribute air throughout the entire house from one central unit. A mini split delivers air directly into specific rooms via wall-mounted units, eliminating the need for ducts and allowing for individual room temperature control.
No, ductless air conditioners do not pull air from outside. They recycle and condition the air already inside your room, filtering it and removing heat/humidity before recirculating it back into the space.
No, a ductless AC system does not create harmful gases and therefore does not need to be vented out of your home like a gas furnace might.
A "ductless house" relies on systems like mini splits or baseboard heaters rather than a central furnace or AC with ductwork. This is common in older historic homes, log cabins, or modern energy-efficient builds.
Yes, each indoor unit contains an air filter that traps dust, pollen, and particulates, helping to purify the air within that specific zone.
No, mini split systems run on electricity and do not burn fuel, so they cannot produce carbon monoxide.
While mini-split systems offer energy-efficient heating and cooling, they may not be the best fit for every home. Upfront installation costs can be higher than some traditional HVAC systems, and multiple indoor units may be needed to condition larger homes. Indoor wall-mounted units are also more visible than conventional ducted systems, which some homeowners may find less appealing. Additionally, regular filter cleaning is important to maintain performance and efficiency.
About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.
About The Expert Reviewer: Manish Chhabra is a Product Manager for Residential Ductless Mini Splits at Carrier Corporation, where he develops innovative comfort solutions designed to meet homeowners' changing needs while aligning with evolving industry standards, energy efficiency goals, and regulatory requirements.