Data Tools
Explore our suite of container refrigeration data tools below
- ML5 Software
- ML3 Software
- MUA Adapter / MST Tool
- DataBank™
- PC Adaptor Card
ML5 Controller Software (PrimeLINE® 571, OptimaLINE™ 701)
Custom-designed ML5 software divides its functionality into configuration and operational performance.
| Unit | Software Version | Configuration File (loaded separately) |
|---|---|---|
| OptimaLINE | 7102 with 251215.cf7 | 260515.cf7 |
| PrimeLINE | 6330 with 251215.cf6 | 260515.cf6 |
This software provides:
- Control supply or return air temperature to required limits, provide modulated refrigeration operation, economized operation, unloaded operation, electric heat control and defrost. Defrost is performed to clear buildup of frost and ice to ensure proper air flow across the evaporator coil.
- Provide default independent readouts of setpoint and supply or return air temperatures.
- Provide ability to read and (if applicable) modify the configuration software variables, operating software function codes and alarm code indications.
- Provide a pre-trip step-by-step checkout of refrigeration unit performance including: proper component operation, electronic and refrigeration control operation, heater operation, probe calibration, pressure limiting and current limiting settings.
- Provide battery-powered ability to access or change selected codes and setpoint without AC power connected. This is only if the carrier-provided rechargeable battery option is installed.
Software Download:
Before downloading the ML5 Software, you agree that you have read and will be bound to the terms and conditions of the End User License Agreement.
To load software: download software below, extract the zip folder and drag the ML5 and configuration files onto a USB.
Note: The latest configuration file is provided in the rightmost column. If it is newer than what is embedded within a release, it will need to be loaded separately. Note: 6325 and before uses .cf5 files while 6326 and later uses .cf6 files. 6393 and above uses .cf7 files.
To load latest configuration: download latest configuration (below), extract zip folder, drag onto a USB.
ML5 Software Loading Procedure
- Place the Start-Stop switch (ST) to “I” to turn the unit On. Wait for controller information to be displayed.
- Insert the USB flash drive, containing controller software, into the controller micro USB port.
- Press the ALT. MODE key on the keypad.
- Use the Arrow keys until “USB” is displayed, then press the ENTER key. (NOTE: If “no USB" is displayed, wait up to 15 seconds for this message to be replaced with a different message. If “no USB" continues to be displayed, remove and insert the USB flash drive and repeat steps 3 and 4.)
- Use the Arrow keys until “UP LOAD” is displayed, then press the ENTER key.
- “LOAD XXXX” is now on the display. If more than one ML5 software revision file is on the USB flash drive at the root level, press the Arrow keys until the correct revision is displayed for the unit. Refer to the table above.
- Press the ENTER key to load the software to the controller.
- When “PULL USB NOW” is displayed, remove the USB drive from the port.
- The following messages will appear to confirm successful programming: “Load Soft” and “Pro Soft” will each appear for several seconds and then “Restart” appears briefly. Then, the controller restarts.
- As the controller starts up, the message “Cd 18” displays the new software loaded and then “Pro done” appears.
Refer to the PrimeLINE or OptimaLINE unit OPERATION AND SERVICE manual for loading the software to the unit.
Manual: T-372 PrimeLINE models 69NT40-571-001 to 199 & 300 to 399. Refer to Section 7.21.2 for procedure.
Manual: T-383 OptimaLINE models 69NT40-701-001 to 199. Refer to Section 7.9.2 for procedure.
Click here for the latest cf5 configuration file (240615.cf5)
Click here to download the tool to load OptimaLINE software onto a PrimeLINE controller (scrl7102.zip)
ML3 Controller Software (ThinLINE®, EliteLINE®, NaturaLINE®, PrimeLINE® 561/565)
The controller software is a custom designed program that is subdivided into configuration software and operational software.
| Unit | Software Version | Configuration File (loaded separately in the "upload" folder) |
| All units for the MST/MUA Tool | See below for Version Numbers | 260315.cf3 |
| EliteLINE / PrimeLINE (NOT TO BE USED ON MAERSK UNITS) | 5391 with 241215.cf3 | 260315.cf3 |
| NaturaLINE | 5716 with 241215.cf3 | 260315.cf3 |
| ThinLINE | 5191 with 241215.cf3 | 260315.cf3 |
The controller software performs the following functions:
- Control supply or return air temperature to required limits, provide modulated refrigeration operation, economized operation, unloaded operation, electric heat control and defrost. Defrost is performed to clear buildup of frost and ice to ensure proper air flow across the evaporator coil.
- Provide default independent readouts of setpoint and supply or return air temperatures.
- Provide ability to read and (if applicable) modify the configuration software variables, operating software function codes and alarm code indications.
- Provide a pre-trip step-by-step checkout of refrigeration unit performance including: proper component operation, electronic and refrigeration control operation, heater operation, probe calibration, pressure limiting and current limiting settings.
- Provide battery-powered ability to access or change selected codes and setpoint without AC power connected. This is only if the carrier-provided rechargeable battery option is installed.
Software download (include all of the copy below and do not change it)
Before downloading the ML3 Software, you agree that you have read and will be bound to the terms and conditions of the End User License Agreement. When loading software, unzip the downloaded file and drag the “carrier” folder onto a USB.
ML3 Software Loading Procedure with MST (07-00572-00)
- Turn unit power off (“0”) at the Start-Stop switch (ST).
- Inspect the pins on the controller’s programming slot for damage.
- Insert the MST tool with USB (with proper software loaded) into the slot.
- Turn unit power on (“I”) at the Start-Stop switch (ST).
- The display will show “USB LOAd”. Use the arrow keys to select "LOAD SOFT" and press the ENTER key.
- Use the Arrow keys until the display shows “LOAD 5XXX” and press the ENTER key.
- The display will alternate between the messages “PRERSS ENTER” and “REV 5XXX”. Press ENTER.
- The display will flash “Pro Soft” as the software is uploading. It may take up to one minute for this to complete. When complete, the display will show “Pro done”. (NOTE: If a problem occurs while loading software, the display will blink the message “Pro FAIL” or “bad 12V.” Turn unit power off “0” at the Start-Stop switch and remove the card.)
- Turn unit power off (“0”) at the Start-Stop switch (ST).
- Remove the programming device from the controller when the LED turns off.
- Turn unit power on (“I”) at the Start-Stop switch (ST).
- On power up, the controller LED flashes quickly and the display will remain blank as the controller loads the new software. This takes about 15 seconds. When complete, the controller will reset and power up normally.
- Bring up function code Cd18 to confirm that the correct software revision is loaded.
Click here to view and download the End User License Agreement
MUA Adapter / MST Tool
Explore two powerful ways to enhance your fleet
The MUA Adapter and MST Tool bring higher efficiency to fleets managed with Micro-Link® 3 (ML3) controllers. Designed by Carrier Transicold, they save time and reduce costs, enabling streamlined interaction with controllers.
- The MUA functions as a pass-through USB device that remains installed in the controller post-setup and is uniquely paired with the unit.
- The MST is a portable USB tool designed to service Carrier units with an ML3 controller, temporarily inserted during maintenance.
Both tools are engineered for reliable support and improved controller usability, ensuring fleet operators experience greater functionality and ease of maintenance.
Click here for ML3 MUA-MST Tools Sell Sheet
Part Numbers:
MUA part number: 07-00571-00PK5
MST part number: 07-00572-00
USB-A* part number: 12-50172-00
Instructions and Downloads
Click here for ML3 USB Adapter 07-00571-00 Instructions
Click here for ML3 Service Tool 07-00572-00 Instructions
Click here for a collection of ML3 software files for the MST/MUA tool
DataBank™ allows for quick trip data analysis and diagnostics.
PC card technology allows you to download most DataCorder™ trip data recorder information in less than 30 seconds.
DataBank™ PC card technology is operationally cost-effective.
- Downloads 30 day, 60 day, 90 day, Trip or All data in 30 seconds or less.
- Frees up valuable time and allows for quick diagnostics analysis.
- Compact design (fits into a pocket) provides a simple and affordable tool to download trip data.
- No special cables or connectors required.
PC Adaptor Card
Delivers the Micro-Link® 3 programming ease to units equipped with Micro-Link 2 and Micro-Link 2i controllers.
Older controllers no longer need to fade into obsolescence. The PC Adaptor Card enables them to benefit from the convenience of newer MicroLink® 3 technology. This adaptor allows the use of ML2 type SRAM cards to load software and configurations, replacing outdated ML2 and ML2i flash memory cards. Additionally, it supports data extraction from ML2i-controlled units using DataBank™ software.