Transform your home comfort
Whole House Humidifiers for Balanced Humidity and Comfort
Discover a reliable way to achieve balanced indoor air quality with Carrier’s range of whole house humidifiers. Designed to seamlessly integrate with your HVAC system, our home humidifiers enhance comfort, protect your house, and improve energy efficiency. Whether you need steam, fan-powered, or bypass humidifiers, Carrier offers advanced solutions tailored to your needs. Installed by a local Carrier expert to integrate with your HVAC systems. Experience the benefits of balanced humidity and explore our innovative products today.
Humidifiers for House: Models & Options
What to look for in a home humidifier
Ensure the humidifier you choose can handle the size of your home. Carrier’s systems are designed to accommodate spaces ranging from 500 to 4,000 square feet, ensuring effective moisture to air distribution throughout your living space.
Tank capacity determines how much water the humidifier can process daily. Carrier humidifiers offer capacities ranging from 11.5 to 34 gallons of water per day, catering to various home sizes and humidity needs.
Run time is crucial for maintaining consistent humidity. This depends on setpoint, home insulation and air sealing, and control strategy. Carrier’s humidifiers can operate for 12 to 24 hours, depending on the model, ensuring continuous comfort throughout the day. Smart control can reduce run time while maintaining comfort.
Budget is an important consideration. Carrier offers a range of humidifiers to fit different price points, from affordable options to premium models. Long-term costs, such as maintenance and energy consumption, should also be factored in.
Balanced humidity levels not only improve comfort but can also help reduce heating costs by making the air feel warmer, allowing you to lower your thermostat settings and save energy.
The right water vapor output depends on your home size and climate. Larger homes or arid climates may require fan-powered or steam humidifiers to add moisture, while bypass humidifiers are sufficient for smaller spaces.
Look for added conveniences like water level indicators, drain indicators, tank empty alerts, and service lights for canister replacement. These precise control features enhance usability and maintenance.
Not sure? What whole home humidifier to get? Talk to a Carrier dealer.
Compare Whole House Humidifiers
Model | HUMCRSTM | HUMCRLBP | HUMCRSBP | HUMCRWBP | HUMCRLFP |
|---|---|---|---|---|---|
Unit Type | Steam | Large bypass | Small bypass | Water saver bypass | Large fan-powered |
Capacity (gallons/day) | 34* | 17 | 12 | 17 | 18 |
Water Vapor Delivery | Dispersion tube in duct | Expanded aluminum evaporator pad | Expanded aluminum evaporator pad | Wicking paper evaporator pad | Expanded aluminum evaporator pad |
Best for | Large homes, highest output | Large homes | Small homes | Efficient in water usage | Large homes |
*Varies based on voltage and amperage.
Humidifier Installation: Seamless integration for optimal performance
Proper installation is essential for the optimal performance of a whole house humidifier. Carrier humidifiers are designed to integrate seamlessly with your HVAC system, delivering even moisture distribution throughout your home. We recommend professional installation to ensure the unit is correctly connected. A typical installation takes several hours and includes mounting the unit, connecting it to your plumbing and electrical systems, setting up the drain line, and configuring the controls. This comprehensive setup ensures efficient operation and minimizes the risk of issues such as leaks or improper humidity levels, letting you enjoy enhanced home comfort with confidence.
Why Carrier
With over a century of leadership in home comfort, Carrier delivers solutions that inspire confidence. We engineer premium whole-house humidifiers designed to integrate seamlessly with your HVAC system, ensuring quiet, efficient performance and enhanced home comfort. Our commitment to innovation is matched only by the reliability of our products and our established network of trusted dealers, ensuring you receive expert service and a system that meets your needs.
Frequently asked questions for choosing the best home humidifier
The best humidifier for a whole house is typically a whole house or centralized humidifier that connects to your HVAC system. When choosing a specific model, consider factors like size, humidification method, coverage area, tank capacity, and features. While your local Carrier expert can recommend the best humidifier for your home based on your individual needs, understanding the core differences between these three types helps you make a confident decision.
- Steam Humidifiers: These units deliver the highest level of performance by boiling water to create steam, which is then dispersed into your ductwork. They operate independently of your furnace activity, making them ideal for larger homes or arid climates requiring precise humidity control. Because they produce their own steam, they offer the most efficient moisture delivery but typically require a dedicated electrical circuit.
- Fan-Powered Humidifiers: These units use an integrated fan to push air across a water-soaked pad, evaporating moisture into the air stream. They are highly effective for medium-to-large homes. They generally require less maintenance than steam units but still offer robust performance.
- Bypass Humidifiers: These systems work by using the furnace's blower to push warm air through the humidifier and back into the return duct. They are efficient, quiet, and simple in design, making them a cost-effective choice for smaller to medium-sized homes. However, they rely on the HVAC system running to operate, so they may not be suitable for homes needing aggressive humidification.
The best place to install a whole house humidifier is typically near the fan coil or furnace in your HVAC system. This location allows the humidifier to efficiently add moisture to the air before it circulates throughout the home. Additionally, ensure it's installed in a location where it can easily access a water supply and drain. Ideally, place it in an area with good airflow, away from obstructions, and close to the return air duct to maximize effectiveness and humidity distribution throughout the house.
The life expectancy of a whole house humidifier depends on the model, usage, and maintenance. Regular maintenance, such as cleaning and replacing filters, can extend its lifespan. Factors like water quality, installation, and overall HVAC system care also influence longevity. Mechanical components may wear out faster if not properly maintained.
When selecting the right humidifier, the first metric you'll encounter is GPD, or gallons per day. This number represents the output capacity of the unit—essentially, how much water it can turn into vapor within 24 hours. Choosing the correct capacity is critical because a unit that is too small won't keep up with demand, while an oversized unit might lead to condensation issues.
Sizing isn't just about square footage; it requires a holistic look at your home’s environment. Key factors include your home’s total size, insulation quality, air leakage (how "tight" your home is), and the local climate.
Here is a simple decision path to help guide your thinking:
- Lower GPD: Typically sufficient for smaller homes, tightly insulated spaces, or regions with milder winters.
- Higher GPD: Necessary for larger homes, older houses with looser insulation, or areas with harsh, dry winters where your heating system runs frequently.
- Maximum Output: For the most precise humidity control and highest capacity, steam humidifiers are the gold standard, capable of delivering significant volume of moisture to air regardless of furnace temperature.
To ensure peak performance and efficiency, we recommend you verify your specific requirements with a Carrier expert. They can account for real-world variables and help you select the perfect Carrier humidifier for your needs. Whether you need a robust steam unit or a reliable bypass system, installing the correct size whole house humidifier ensures your family stays comfortable all winter long.
Yes, effective humidity control requires smart water management, though the specific needs depend on the technology you choose. Steam humidifiers boil water to create water vapor and typically require a drain connection to flush out mineral deposits and ensure long-term reliability. Flow-through models, such as fan-powered and standard bypass units, continuously rinse the evaporator pad to add moisture to the air; any water that doesn't evaporate is drained away to keep the system clean.
For those prioritizing efficiency, a water-saver bypass design is an excellent option that reduces water consumption while maintaining optimal home comfort. The amount of water your system uses—and subsequently drains—is also influenced by your water hardness and control strategy, which can impact maintenance frequency.
Typically, the drain line integrates seamlessly with your existing condensate drain near the furnace blower or air handler. We recommend having a carrier dealer confirm your home's drain availability, routing, and code compliance to ensure your system performs perfectly for years to come.
Yes, professional installation is the best way to ensure your system delivers optimal performance and reliability from day one. A furnace humidifier is more than an appliance; it's an integrated component of your home's HVAC systems. Proper installation requires precise plumbing, electrical, and ductwork integration that demands expert training and also protects your warranty coverage.
On installation day, you can expect a comprehensive setup that is typically completed in just a few hours. The process includes:
- Mounting the unit securely
- Connecting the water supply and drain line (if applicable)
- Wiring the system and configuring the controls
- Performing a thorough leak check
- Calibrating the system for ideal humidity control
A professional ensures all work is compliant with local codes and that all routing is clean and secure. At handoff, your local Carrier expert will also review the ongoing maintenance schedule, such as pad or canister replacement, to help you sustain perfect humidity levels and peak performance for years to come.